build errors on MIMXRT685-EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

build errors on MIMXRT685-EVK

1,324 Views
BobWang3
Contributor I

Hello,

We are developing DSP and MCU SW on MIMXRT685-EVK, but when I include more DSP codes (when DSP bin size is over about 500KB), build result will be failed with below errors: (dangerous relocation: call8: call target out of range: memcpy)

########################################debug log###

 STD: cmd.exe /C "cd . && C:/usr/xtensa/XtDevTools/install/tools/RI-2020.5-win32/XtensaTools/bin/xt-xc++.exe --xtensa-core=nxp_rt600_RI2020_5_xclib -std=c++11 -clang -D__hifi4__ -DBUILD_HIFI4 @CMakeFiles\app.rsp -o ..\bin\debug\app.elf -mlsp=C:/NXP_HiFi4/hifi4_platform/build/cmake/../../sdk/SDK_2.9.0_EVK-MIMXRT685/xtensa/gdbio && cmd.exe /C "cd /D C:\NXP_HiFi4\hifi4_platform\code\hifi4\output\bhifi4_debug\hifi4\dapp\src && C:\usr\xtensa\XtDevTools\install\tools\RI-2020.5-win32\XtensaTools\bin\xt-objcopy.exe --xtensa-params= -Obinary C:/NXP_HiFi4/hifi4_platform/build/cmake/../../code/hifi4/output/bin/debug/app.elf C:/NXP_HiFi4/hifi4_platform/build/cmake/../../code/hifi4/output/bin/debug/dsp_text_debug.bin --xtensa-core=nxp_rt600_RI2020_5_xclib --only-section=.dram0.rodata --only-section=.Level2InterruptVector.literal --only-section=.Level3InterruptVector.literal --only-section=.DebugExceptionVector.literal --only-section=.NMIExceptionVector.literal --only-section=.KernelExceptionVector.literal --only-section=.UserExceptionVector.literal --only-section=.DoubleExceptionVector.literal --only-section=.iram0.literal --only-section=.ResetVector.literal --only-section=.dram0.literal --only-section=.dram0.data --only-section=.dram0.bss --only-section=.ResetVector.text --only-section=.ResetHandler.literal --only-section=.ResetHandler.text --only-section=.WindowVectors.text --only-section=.Level2InterruptVector.text --only-section=.Level3InterruptVector.text --only-section=.DebugExceptionVector.text --only-section=.NMIExceptionVector.text --only-section=.KernelExceptionVector.text --only-section=.UserExceptionVector.text --only-section=.DoubleExceptionVector.text --only-section=.iram0.text && cd /D C:\NXP_HiFi4\hifi4_platform\code\hifi4\output\bhifi4_debug\hifi4\dapp\src && C:\usr\xtensa\XtDevTools\install\tools\RI-2020.5-win32\XtensaTools\bin\xt-objcopy.exe --xtensa-params= -Obinary C:/NXP_HiFi4/hifi4_platform/build/cmake/../../code/hifi4/output/bin/debug/app.elf C:/NXP_HiFi4/hifi4_platform/build/cmake/../../code/hifi4/output/bin/debug/dsp_data_debug.bin --xtensa-core=nxp_rt600_RI2020_5_xclib --only-section=.text --only-section=.rodata --only-section=.data --only-section=.bss --only-section=.literal --only-section=.sram.text --only-section=.sram.rodata --only-section=.sram.data --only-section=.sram.bss --only-section=.sram.literal --only-section=.clib.rodata --only-section=.clib.text --only-section=.clib.data --only-section=.clib.percpu.data --only-section=.clib.bss --only-section=.clib.percpu.bss --only-section=.clib.literal --only-section=.rtos.rodata --only-section=.rtos.text --only-section=.rtos.data --only-section=.rtos.percpu.data --only-section=.rtos.bss --only-section=.rtos.percpu.bss --only-section=.rtos.literal && cd /D C:\NXP_HiFi4\hifi4_platform\code\hifi4\output\bhifi4_debug\hifi4\dapp\src && C:\usr\xtensa\XtDevTools\install\tools\RI-2020.5-win32\XtensaTools\bin\xt-objcopy.exe --xtensa-params= -Obinary C:/NXP_HiFi4/hifi4_platform/build/cmake/../../code/hifi4/output/bin/debug/app.elf C:/NXP_HiFi4/hifi4_platform/build/cmake/../../code/hifi4/output/bin/debug/dsp_ncache_debug.bin --xtensa-core=nxp_rt600_RI2020_5_xclib --only-section=NonCacheable""
STD: hifi4\dapp\src\CMakeFiles\app.dir\debug.cpp.obj: In function `output_debug_trace(char const*)':
STD: C:\NXP_HiFi4\hifi4_platform\code\hifi4\dapp\src/debug.cpp:96:(.text+0xa2): dangerous relocation: call8: call target out of range: memcpy
STD: hifi4\dapp\src\CMakeFiles\app.dir\debug.cpp.obj: In function `rpmsg_log(char const*)':
STD: C:\NXP_HiFi4\hifi4_platform\code\hifi4\dapp\src/debug.cpp:61:(.text+0x19a): dangerous relocation: call8: call target out of range: memcpy
STD: ninja: build stopped: subcommand failed.

###############################################

But I have already set the DSP core start address with 0x00200000, and len with 0x280000.

I think the SRAM size is enough, but when I tried to delete some DS code and make the DSP bin size below about 500KB, it will has no build errors.

 

 

I have tried to adjust the memory setting, but cannot fix this issue.

Could you help to check it?

 

0 Kudos
Reply
1 Reply

1,309 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

There is also other code or data need SRAM, for example memcpy, please pay attention the below compile log:

 

STD: hifi4\dapp\src\CMakeFiles\app.dir\debug.cpp.obj: In function `output_debug_trace(char const*)':
STD: C:\NXP_HiFi4\hifi4_platform\code\hifi4\dapp\src/debug.cpp:96:(.text+0xa2): dangerous relocation: call8: call target out of range: memcpy
STD: hifi4\dapp\src\CMakeFiles\app.dir\debug.cpp.obj: In function `rpmsg_log(char const*)':
STD: C:\NXP_HiFi4\hifi4_platform\code\hifi4\dapp\src/debug.cpp:61:(.text+0x19a): dangerous relocation: call8: call target out of range: memcpy

 

 

BR

Alice

0 Kudos
Reply