booting i.MX6 UL custom board using usb_loader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

booting i.MX6 UL custom board using usb_loader

1,383件の閲覧回数
arunachalamrama
Contributor III

I am trying to boot i.MX6 UL Custom Board using usb_loader.

Given below is the configuration I use:

mx6_qsb

#hid/bulk,[old_header,]max packet size, dcd_addr, {ram start, ram size}(repeat valid ram areas)
#hid,1024,0x910000,0x10000000,1G,0x00900000,0x40000  << original value

hid,1024,0x910000,0x08000000,512M,0x00900000,0x40000 << modified for UL Custom Board with 512MB memory

u-boot-sd-2016.03-r0.imx:dcd,plug
zImage--4.1.15-r0-imx6ulcustbrd-20170322082522.bin:load 0x80800000
xyz-image-imx6ulcustbrd.rootfs.cpio.gz.u-boot:load 0x83800000
zImage--4.1.15-r0-imx6ulcustbrd-20170322082522.dtb:load 0x83000000
u-boot-sd-2016.03-r0.imx:clear_dcd,jump header

Are the updated values for following are correct?

dcd_addr, {ram start, ram size}(repeat valid ram areas)

Please explain more about these variables.

タグ(1)
0 件の賞賛
返信
1 返信

1,013件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Arunachalam

some usb_loader documentation and sources can be found on

AdeneoEmbedded - Whitepaper on USB loader for i.MX6 platforms 

GitHub - boundarydevices/imx_usb_loader: Usb loader for imx51/53/6x 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信