booti fails to initialize and run android

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

booti fails to initialize and run android

4,370 Views
oussama
Contributor III

I've using android 4.4.2/imx6. I've installed boot.img and system.img in sdX1 and sdX5. I do not using the recovery.img.

I've set the bootargs to  'console=ttymxc0,115200n8 earlyprintk vmalloc=400M  video=mxcfb0:dev=ldb,LDB-AM-800480STMQW-TA1,if=RGB666 ldb=sin0 init=/init androidboot.console=ttymxc0 androidboot.hardware=freescale'

Then I tried to boot with booti mmc0

The kernel boots successfully as you can see here:

U-Boot > booti mmc0

booti mmc0

kernel   @ 10808000 (4047468)

ramdisk  @ 11800000 (499651)

kernel cmdline:

  use boot.img command line:

  console=ttymxc0,115200n8 earlyprintk vmalloc=400M  video=mxcfb0:dev=ldb,LDB-AM-800480STMQW-TA1,if=RGB666 ldb=sin0 init=/init androidboot.console=ttymxc0 androidboot.hardware=freescale

No gpc device node -9, force to ldo-enable.

Power: using LDO mode!

Using machid 0x1308 from environment

Starting kernel ...

Uncompressing Linux... done, booting the kernel.


But then, it fails to init the system

[    7.395345] VFS: Cannot open root device "(null)" or unknown-block(0,0)

[    7.401964] Please append a correct "root=" boot option; here are the available partitions:

[    7.410351] 1f00           32768 mtdblock0  (driver?)

[    7.415439] 1f01          524288 mtdblock1  (driver?)

[    7.420511] b300         1931264 mmcblk0  driver: mmcblk

[    7.425866]   b301            9455 mmcblk0p1 00000000-0000-0000-0000-000000000000

[    7.433385]   b302            9455 mmcblk0p2 00000000-0000-0000-0000-000000000000

[    7.442918]   b303               1 mmcblk0p3 00000000-0000-0000-0000-000000000000

[    7.452506]   b304          798555 mmcblk0p4 00000000-0000-0000-0000-000000000000

[    7.460022]   b305          525697 mmcblk0p5 00000000-0000-0000-0000-000000000000

[    7.469559]   b306          525697 mmcblk0p6 00000000-0000-0000-0000-000000000000

[    7.479088]   b307            9454 mmcblk0p7 00000000-0000-0000-0000-000000000000

[    7.488619]   103:00000       9454 mmcblk0p8 00000000-0000-0000-0000-000000000000

[    7.498153] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)

Labels (2)
Tags (3)
0 Kudos
Reply
4 Replies

3,243 Views
igorpadykov
NXP Employee
NXP Employee

Hi oussama

seems you missed to add kernel parameter "root" (indicates the

location of the root file system). Please check attached

Android_User's_Guide.pdf 5.4.2 Kernel command line from

IMX6_KK442_100_ANDROID_DOCS

also you may wish to try more new android 4.4.3

MX6_KK443_200_ANDROID_SOURCE_BSP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,243 Views
simon_cai
Contributor III

hi igorpadykov

I have downloaded the KK4.4.3 BSP.

but where I can fetch the documents for reference, something like IMX6_KK443_200_ANDROID_DOCS

Thanks

Bateman

0 Kudos
Reply

3,243 Views
igorpadykov
NXP Employee
NXP Employee

Hi bateman

<https://www.freescale.com/webapp/Download?colCode=IMX6_KK443_200_ANDROID_DO

CS&location=null&fasp=1&WT_TYPE=Supporting%20Information&WT_VENDOR=FREESCALE

&WT_FILE_FORMAT=gz&WT_ASSET=Documentation&fileExt=.gz>

IMX6_KK443_200_ANDROID_DOCS

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q

<http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&nodeI

d=018rH3ZrDRB24A&fpsp=1&tab=Documentation_Tab>

&nodeId=018rH3ZrDRB24A&fpsp=1&tab=Documentation_Tab

Best regards

igor

0 Kudos
Reply

3,243 Views
simon_cai
Contributor III

hi igorpadykov

thanks for you support.

I have got it.

thanks

Bateman

0 Kudos
Reply