boot the bootanimation as early as possible?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

boot the bootanimation as early as possible?

1,034 Views
yunyangsihai
Contributor II

Dear guys:

Platform:iMX6 DualLite + BSP-3.10.53 + bootanimation(with sound)。

1.Now, I boot the animation with gstreamer-0.1, it takes too long to start the udev , load the gstreamer codec, load the vpu

firmware and so on before show the first frame.

2. Some useful ideas: optimize the boot time; or intergrate part of the animation to the kernel; or replace gstreamer with something else?

3.animation: MPEG-4 MPEG-4, x264 core.

It takes about 9~10 second to show the first frame now. How could i boot the animation(with sound) after power up as early as possible ?

Thanks anyway.

Labels (3)
0 Kudos
Reply
1 Reply

894 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi yang,

You can optimize the booting process. You can make it by re-arranging the booting process and eliminating some unnecessary process for the booting.

However, you can go with NXP professional service support and they can help you make a patch:

NXP Professional Services|NXP 

0 Kudos
Reply