boot partition in SD card and rootfs in the USB flash disk

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

boot partition in SD card and rootfs in the USB flash disk

3,940 次查看
HEXER
Contributor III

Greetings community.

I am using i.MX8 MQ based MaaXBoard. It has SD card slot and USB 3.0 ports. I want to prepare a system such that boot partition will be in the SD card and rootfs will be in the USB flash disk.

I can write only u-boot to the SD card and use it on my development board.

I can use yocto build system and generate yocto images (bootloader, rootfs etc) but i dont know how to achieve above goal. I can use u-boot command line and i think it is possible to achieve this using u-boot command line.

 

Could you give me the some command so i can boot from SD card and install footfs to my usb flash disk so that u-boot read my usb flash disk which includes rootfs.

 

Best regard and sorry for my bad english.

0 项奖励
回复
5 回复数

3,889 次查看
smithcoba
Contributor III

1. You need to prepare usb the same as you prepare sdcard. 

2, The you use the following commands

usb reset

fatls usb 0:1

fatload usb 0:1 ${fdt_addr} imx8mm-evk.dtb


fatload usb 0:1 ${loadaddr} ${image}

setenv bootargs console=${console},${baudrate} ${smp} root=/dev/sda2 rootwait rw

booti ${loadaddr} - ${fdt_addr_r}

If you use mount command, you will see the rootfs is usb sda2.(default emmc is /dev/mmcblk2p2 on / type ext4 (rw,relatime))

/dev/sda2 on / type ext4 (rw,relatime)

 

root@imx8mmevk:~#
root@imx8mmevk:~# mount
/dev/sda2 on / type ext4 (rw,relatime)
devtmpfs on /dev type devtmpfs (rw,relatime,size=668780k,nr_inodes=167195,mode=755)

 

3,823 次查看
HEXER
Contributor III

First, Thank you for your response.

I think these commands what i needed.

I am going to give it a try and i am going to inform you about the result and possible errors.

Best regards.

0 项奖励
回复

3,899 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi @HEXER 

I think that you can refer to the "4.3.6 Copying the root file system (rootfs)" from i.MX Linux User's Guide (nxp.com) which documents with detailed commands.

 

Best regards

Harvey

0 项奖励
回复

3,841 次查看
smithcoba
Contributor III

Harvey,

I checked the 4.3.6 Copying the root file system (rootfs) the document in the link you provided, there are no details information about the bootloader on emmc but rootfs on usb, which you said "documents with detailed commands".

Could you please kindly highlight, better to take picture of those detailed commands?

3,820 次查看
HEXER
Contributor III

i agree, there was no rootfs on usb related commands

0 项奖励
回复