boot logo in animation imx6 sololite

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

boot logo in animation imx6 sololite

1,677 Views
kondaveetiarung
Contributor II

Hi currently iam working on imx6 sololite.i want to play animation boot up logo in the u-boot.Please tell me how to do it in kernel level and u-boot.Please tell me any inputs

0 Kudos
4 Replies

961 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi kondaveeti,

in the u-boot release note you can find instructions to change the splash screen, but setting an animation is not supported by u-boot. You may need to make edition in u-boot source and this is not part of the free support scope. If you are interested in getting paid support you may contact www.nxp.com/services


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

961 Views
kondaveetiarung
Contributor II

Hi,

Thank you for your valuable reply.Normally in mobiles it is showing animated gifs or videos these types are handled in kernel or u-boot?

i want to add those type of animation in imx6 sololite processor.

Please tell me how to do this?

0 Kudos

961 Views
Carlos_Musich
NXP Employee
NXP Employee

Are you using Linux or Android?

Carlos

0 Kudos

961 Views
kondaveetiarung
Contributor II

Hi Carlos_Musich,

Sorry for late reply.Thank you for your reply.

Iam using linux 3.10.17 kernel.

0 Kudos