boot from nand

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

boot from nand

4,522 次查看
enaud
Contributor III

Hi,

how is possible flash nand (with uboot.bin, uImage and rootfs) and start without SD but only from nand?

thanks

标签 (1)
0 项奖励
回复
7 回复数

4,060 次查看
enaud
Contributor III

QSB

0 项奖励
回复

4,060 次查看
KrishnaPavan
Contributor II

Is it QSB or SABRE or ARD or EVK etc etc.?

enaud said:

imx53

0 项奖励
回复

4,060 次查看
enaud
Contributor III

imx53

0 项奖励
回复

4,060 次查看
KrishnaPavan
Contributor II

Which board are you using?

0 项奖励
回复

4,060 次查看
DirkBehme
Contributor III

You might want to have a look to

http://imxcommunity.org/forum/topics/cannot-boot-from-nand

The discussion there is about the i.MX53 ARD board, but some parts might help for the QSB, too.

0 项奖励
回复

4,060 次查看
positron
Contributor I

Hello, Not only the hardware connection. You need to change the imximage.cfg (for u-boot) configurations to make it boot from NAND. If you are looking for a one-line answer on how to boot from NAND, I'd say "It is not that easy". You need to study the manual, patch in the IOMUX settings, write imximage.cfg, tweak the board file. Do it one step at a time.

0 项奖励
回复

4,057 次查看
jomeke
Contributor II

Hi Enaud,

you can find the information in the user manual under chapter 7.

I have made a summary in the Excel file attached.

Have a look

0 项奖励
回复