boot from USDHC-1 with SD card.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

boot from USDHC-1 with SD card.

834 次查看
kimsuhak
Contributor I

Hello

we are working on IMX6Q AI board.

the origin IMX6Q board is booting with SD card( USDHC-3).

We want change boot mode from USDHC-3 to  USDHC-1. Still use SD card.

But bootloader 4K is not dump to Internal RAM.

Is that possible to boot from SD card on USDHC-1?

Is there anyone who has experience to develop board just like that?

help me

0 项奖励
回复
1 回复

580 次查看
igorpadykov
NXP Employee
NXP Employee

Hi kim

please look at links below

booting from SD1

Linux Software User Manual (i.MX6) - BlueWiki

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复