bluetoothctl is not working with 8MMINILPD4-EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

bluetoothctl is not working with 8MMINILPD4-EVK

ソリューションへジャンプ
4,201件の閲覧回数
Takashi_Kashiwagi
Senior Contributor I

Hi everyone.

Do I need any special settings to use Bluetooth on 8MMINILPD4-EVK?

I bought 8MMINILPD4-EVK last week, and I bitbaked "fsl-image-qt5-validation-imx" (4.14-sumo). 

I did some functional checks, but I noticed that bluetoothctl returns "No default controller available".

root@imx8mmevk:~# bluetoothctl
Agent registered
[bluetooth]# devices
No default controller available
[bluetooth]# scan on
No default controller available
[bluetooth]# power on
No default controller available
[bluetooth]# version
Version 5.49
[bluetooth]# quit
root@imx8mmevk:~#

I think that some settings are missing, does anyone know correct settings?

-- more information --

I checked dmseg, The HCI manager looks fine, but hciconfig can not find the device.

root@imx8mmevk:~# dmesg | grep "Bluetooth"
[ 0.874063] Bluetooth: Core ver 2.22
[ 0.881586] Bluetooth: HCI device and connection manager initialized
[ 0.887969] Bluetooth: HCI socket layer initialized
[ 0.892866] Bluetooth: L2CAP socket layer initialized
[ 0.897954] Bluetooth: SCO socket layer initialized
[ 2.027685] Bluetooth: HCI UART driver ver 2.3
[ 2.032149] Bluetooth: HCI UART protocol H4 registered
[ 2.037297] Bluetooth: HCI UART protocol BCSP registered
[ 2.042617] Bluetooth: HCI UART protocol ATH3K registered
[ 2.048024] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 2.054441] Bluetooth: HCI UART protocol Broadcom registered
[ 2.060112] Bluetooth: HCI UART protocol QCA registered
[ 2.752373] Bluetooth: RFCOMM TTY layer initialized
[ 2.752385] Bluetooth: RFCOMM socket layer initialized
[ 2.752401] Bluetooth: RFCOMM ver 1.11
[ 2.752407] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 2.752410] Bluetooth: BNEP filters: protocol multicast
[ 2.752415] Bluetooth: BNEP socket layer initialized
[ 2.752418] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 2.752423] Bluetooth: HIDP socket layer initialized
root@imx8mmevk:~# hciconfig
root@imx8mmevk:~# hci
hciattach hcidump hcisecfilter
hciconfig hcieventmask hcitool
root@imx8mmevk:~# sudo hciconfig hci0 up
Can't get device info: No such device
root@imx8mmevk:~#

----

Best Regards,

T.Kashiwagi

ラベル(3)
タグ(1)
1 解決策
3,591件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I got reply for the imx8M board, maybe you can refer to it:

"To use the Bluetooth, try setting up the ttymxc2 device with the below command:

hciattach /dev/ttymxc2 qca

 

After that, use the hcitool Linux tool to set up the Bluetooth connection between two devices."

元の投稿で解決策を見る

4 返答(返信)
3,592件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I got reply for the imx8M board, maybe you can refer to it:

"To use the Bluetooth, try setting up the ttymxc2 device with the below command:

hciattach /dev/ttymxc2 qca

 

After that, use the hcitool Linux tool to set up the Bluetooth connection between two devices."

3,591件の閲覧回数
Takashi_Kashiwagi
Senior Contributor I

Hi Joan

Thank you for responding!

I executed "hciattach /dev/ttymxc0 qca", and "Device setup complete" was printed. 

Also bluetoothctl worked. Thank you for your advise!

root@imx8mmevk:~# hciconfig
hci0: Type: Primary Bus: UART
BD Address: 61:47:AA:32:44:06 ACL MTU: 1024:7 SCO MTU: 60:8
UP RUNNING
RX bytes:781 acl:0 sco:0 events:50 errors:0
TX bytes:2472 acl:0 sco:0 commands:50 errors:0

root@imx8mmevk:~#

root@imx8mmevk:~# bluetoothctl
Agent registered
[bluetooth]# scan on
Discovery started
[CHG] Controller 61:47:AA:32:44:06 Discovering: yes

.

.

.

.

Best Regards,

T.kashiwagi

0 件の賞賛
返信
3,591件の閲覧回数
abdu1
Contributor I

Hi

I am facing the same issues with my IMX8M Mini board. I have tried doing everything on this thread, one thing i am not able to do, is using hciattach command. I suspect i am doing something wrong. Since i am very new to this, can someone please elaborate on using the hciattach command to turn bluetooth ON? I get the following error when i try to run the hciattach command.

 

evk_8mm:/ # 
evk_8mm:/ # hciattach 
/system/bin/sh: hciattach: not found 
127|evk_8mm:/ # hciattach /dev/ttymxc2 qca 
/system/bin/sh: hciattach: not found


Regards

Abdu

0 件の賞賛
返信
3,591件の閲覧回数
Takashi_Kashiwagi
Senior Contributor I

Hi Abdu

I think “hciattach” is a BlueZ command. Looking at the contents of the error, it seems that there is no “hciattach”.

Please Make sure BlueZ is included when you bitbake.

Best Regards,

T.kashiwagi

0 件の賞賛
返信