blhost cannot connect MIMXRT1064 EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

blhost cannot connect MIMXRT1064 EVK

ソリューションへジャンプ
1,153件の閲覧回数
martinzhang
Contributor III

Hi,

I configure the boot mode in MIMIXRT1064 EVK as: 0x01, and use following command to connect MCU via COM1 in PC side:

blhost -p COM1 -- get-property 10

got response:

Error: Initial ping failure: No response received for ping command.

 

I have confirmed the boot mode in register:

BootModeReg.png

 and COM1 is working:

COM1_OK.png

Also, according the schematic of the MIMXRT1064 EVK, the pins of UART1 is same with the boot loader

UART1_Setting.png

 

Someone can tell me where I missed?

Best Regards,

Martin

ラベル(1)
0 件の賞賛
返信
1 解決策
1,149件の閲覧回数
Yuri
NXP Employee
NXP Employee

@martinzhang 
Hello,

   The blhost application is a command-line utility used on the host computer to initiate communication and inject commands to the MCU bootloader. The MCU bootloader is not boot ROM , it should be preloaded first, using the sdphost. Please refer to app note AN12238 (i.MX RT1050 Flashloader use cases) for more details.

https://www.nxp.com/docs/en/nxp/application-notes/AN12238.pdf

 

Regards,
Yuri.

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,150件の閲覧回数
Yuri
NXP Employee
NXP Employee

@martinzhang 
Hello,

   The blhost application is a command-line utility used on the host computer to initiate communication and inject commands to the MCU bootloader. The MCU bootloader is not boot ROM , it should be preloaded first, using the sdphost. Please refer to app note AN12238 (i.MX RT1050 Flashloader use cases) for more details.

https://www.nxp.com/docs/en/nxp/application-notes/AN12238.pdf

 

Regards,
Yuri.

 

0 件の賞賛
返信