black screen in HDMI output when typing in terminal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

black screen in HDMI output when typing in terminal

Jump to solution
2,046 Views
jojorong
Contributor IV

Hi,

     The screen is black suddenly when typing in the terminal in small probability, i use the yocto project to create image with stable brach dylan,

     it is black almost if you use the application called "virt-viewer" or "spice-gtk" with FSL driver.

     This is not happen without any FSL driver with image "core-image-sato" or "core-image-sato-sdk",

     anyone have any advices ? thanks so much

Labels (4)
0 Kudos
Reply
1 Solution
1,855 Views
jojorong
Contributor IV

This issue is fixed in yocto dora branch looks like :smileyhappy:

View solution in original post

0 Kudos
Reply
2 Replies
1,855 Views
OtavioSalvador
Senior Contributor II

Sorry but I didn't get the problem you have. Can you describe it a little bit more descriptive?

0 Kudos
Reply
1,856 Views
jojorong
Contributor IV

This issue is fixed in yocto dora branch looks like :smileyhappy:

0 Kudos
Reply