bitbake yocto question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

bitbake yocto question

1,392 次查看
hnxylhb
Contributor I

WARNING: Failed to fetch URL http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-test-hdcp-3.10.17-1.0.0.bin;fsl-eula=true, attempting MIRRORS if available

ERROR: Fetcher failure: Fetch command failed with exit code 8, output:

http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-test-hdcp-3.10.17-1.0.0.bin:

2015-07-13 09:22:58 ERROR 404: Not Found.

ERROR: Function failed: Fetcher failure for URL: 'http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-test-hdcp-3.10.17-1.0.0.bin;fsl-eula=true'. Unable to fetch URL from any source.

ERROR: Logfile of failure stored in: /home/jishuxing/fsl-arm-yocto-bsp/build/tmp/work/riotboard-poky-linux-gnueabi/imx-test-hdcp/3.10.17-1.0.0-r0/temp/log.do_fetch.3692

ERROR: Task 1667 (/home/jishuxing/fsl-arm-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/imx-test/imx-test-hdcp_3.10.17-1.0.0.bb, do_fetch) failed with exit code '1'

NOTE: Tasks Summary: Attempted 2351 tasks of which 2350 didn't need to be rerun and 1 failed.

No currently running tasks (2350 of 4013)

标签 (2)
0 项奖励
回复
1 回复

939 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello roc li,

Would you please provide more information on this error? Which BSP are you using and which images or packages are you baking? I’m curious because the binaries are not being downloaded from the gits but from Freescale.com

0 项奖励
回复