Hello, I'm trying to build qt5 toolchain for sabresd board but it fails. I was able to build cross-compile toolchain (bitbake meta-toolchain) and rootfs image (bitbake fsl-image-qt5).
It appears that the main reason is:
ERROR: Function failed: Fetcher failure for URL: 'git://qt.gitorious.org/qt/qtsystems.git;branch=dev'. Unable to fetch URL from any source.
If somebody could comment or recommend a solution that would be great.
Below are details:
$ cat conf/local.conf
BB_NUMBER_THREADS ?= "${@oe.utils.cpu_count()}"
PARALLEL_MAKE ?= "-j ${@oe.utils.cpu_count()}"
MACHINE ??= 'imx6qsabresd'
DISTRO ?= 'poky'
PACKAGE_CLASSES ?= "package_rpm"
EXTRA_IMAGE_FEATURES = "debug-tweaks"
USER_CLASSES ?= "buildstats image-mklibs image-prelink"
PATCHRESOLVE = "noop"
BB_DISKMON_DIRS = "\
STOPTASKS,${TMPDIR},1G,100K \
STOPTASKS,${DL_DIR},1G,100K \
STOPTASKS,${SSTATE_DIR},1G,100K \
ABORT,${TMPDIR},100M,1K \
ABORT,${DL_DIR},100M,1K \
ABORT,${SSTATE_DIR},100M,1K"
PACKAGECONFIG_pn-qemu-native = "sdl"
PACKAGECONFIG_pn-nativesdk-qemu = "sdl"
ASSUME_PROVIDED += "libsdl-native"
CONF_VERSION = "1"
BB_NUMBER_THREADS = '4'
PARALLEL_MAKE = '-j 4'
DL_DIR ?= "${BSPDIR}/downloads/"
ACCEPT_FSL_EULA = ""
PREFERRED_PROVIDER_virtual/mesa = ""
DISTRO_FEATURES_remove = "x11 wayland directfb "
IMAGE_INSTALL_append = " \
qtquickcontrols-qmlplugins \
"
PACKAGECONFIG_append_pn-qtquickcontrols = " accessibility"
PACKAGECONFIG_append_pn-qtbase = " accessibility"
$ bitbake meta-toolchain-qt5
Loading cache: 100% |###########################################################################################################| ETA: 00:00:00
Loaded 2185 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies
NOTE: multiple providers are available for jpeg (jpeg, libjpeg-turbo)
NOTE: consider defining a PREFERRED_PROVIDER entry to match jpeg
NOTE: multiple providers are available for runtime libgl-mesa-dev (mesa, mesa-gl)
NOTE: consider defining a PREFERRED_PROVIDER entry to match libgl-mesa-dev
NOTE: multiple providers are available for runtime libglapi (mesa, mesa-gl)
NOTE: consider defining a PREFERRED_PROVIDER entry to match libglapi
Build Configuration:
BB_VERSION = "1.22.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-12.04"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6qsabresd"
DISTRO = "poky"
DISTRO_VERSION = "1.6.2"
TUNE_FEATURES = "armv7a vfp neon callconvention-hard cortexa9"
TARGET_FPU = "vfp-neon"
meta
meta-yocto = "(nobranch):30b8d9378b8260e452552b806610dc9b6fe0b69f"
meta-oe = "(nobranch):8065dd8456913457a0114ddb2b4bd4842847b2a3"
meta-fsl-arm = "(nobranch):9bc540eec9a7e280af13371ea70650fcc47ea627"
meta-fsl-arm-extra = "(nobranch):e1085deb3d915d2a95a65cceadc77c6de0dadfb6"
meta-fsl-demos = "(nobranch):f141c7d1158b8addbd6f1ed047a1b47c2ed85f8f"
meta-fsl-arm
meta-fsl-demos = "(nobranch):e6f24ebca19440924b7bf485974710ee0338ea57"
meta-browser = "(nobranch):63963cc56c8d0291779693e62b66cb16e5c86883"
meta-gnome
meta-networking
meta-ruby = "(nobranch):8065dd8456913457a0114ddb2b4bd4842847b2a3"
meta-qt5 = "(nobranch):c29c317e0f22202bfaa85329a580564bbc179089"
meta-fsl-qt5
meta-fsl-bluez = "(nobranch):e6f24ebca19440924b7bf485974710ee0338ea57"
NOTE: Preparing runqueue
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
WARNING: Failed to fetch URL git://qt.gitorious.org/qt/qtsystems.git;branch=dev, attempting MIRRORS if available
ERROR: Fetcher failure: Fetch command failed with exit code 128, output:
Cloning into bare repository '/home/dostojic/sabresd_yocto/downloads//git2/qt.gitorious.org.qt.qtsystems.git'...
fatal: The remote end hung up unexpectedly
ERROR: Function failed: Fetcher failure for URL: 'git://qt.gitorious.org/qt/qtsystems.git;branch=dev'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/dostojic/sabresd_yocto/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/qtsystems/5.2.1+gitAUTOINC+aa651c73bf-r0/temp/log.do_fetch.21821
ERROR: Task 814 (/home/dostojic/sabresd_yocto/sources/meta-qt5/recipes-qt/qt5/qtsystems_git.bb, do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 1927 tasks of which 1917 didn't need to be rerun and 1 failed.
Waiting for 0 running tasks to finish:
Summary: 1 task failed:
/home/dostojic/sabresd_yocto/sources/meta-qt5/recipes-qt/qt5/qtsystems_git.bb, do_fetch
Summary: There was 1 WARNING message shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.
Solved! Go to Solution.
Please, repo sync
the patch was included in the tree:
meta-fsl-bsp-release.git - Freescale i.MX Yocto BSP Release Layer
Please, repo sync
the patch was included in the tree:
meta-fsl-bsp-release.git - Freescale i.MX Yocto BSP Release Layer
Hi Daiane, this made it work.
Thanks, Dragan