bitbake meta-toolchain-qt5 fails for imx-3.10.53_1.1.0_ga

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

bitbake meta-toolchain-qt5 fails for imx-3.10.53_1.1.0_ga

Jump to solution
2,992 Views
DraganOstojic
Contributor V

Hello, I'm trying to build qt5 toolchain for sabresd board but it fails. I was able to build cross-compile toolchain (bitbake meta-toolchain) and rootfs image (bitbake fsl-image-qt5).

It appears that the main reason is:

ERROR: Function failed: Fetcher failure for URL: 'git://qt.gitorious.org/qt/qtsystems.git;branch=dev'. Unable to fetch URL from any source.

If somebody could comment or recommend a solution that would be great.

Below are details:

$ cat conf/local.conf

BB_NUMBER_THREADS ?= "${@oe.utils.cpu_count()}"

PARALLEL_MAKE ?= "-j ${@oe.utils.cpu_count()}"

MACHINE ??= 'imx6qsabresd'

DISTRO ?= 'poky'

PACKAGE_CLASSES ?= "package_rpm"

EXTRA_IMAGE_FEATURES = "debug-tweaks"

USER_CLASSES ?= "buildstats image-mklibs image-prelink"

PATCHRESOLVE = "noop"

BB_DISKMON_DIRS = "\

    STOPTASKS,${TMPDIR},1G,100K \

    STOPTASKS,${DL_DIR},1G,100K \

    STOPTASKS,${SSTATE_DIR},1G,100K \

    ABORT,${TMPDIR},100M,1K \

    ABORT,${DL_DIR},100M,1K \

    ABORT,${SSTATE_DIR},100M,1K"

PACKAGECONFIG_pn-qemu-native = "sdl"

PACKAGECONFIG_pn-nativesdk-qemu = "sdl"

ASSUME_PROVIDED += "libsdl-native"

CONF_VERSION = "1"

BB_NUMBER_THREADS = '4'

PARALLEL_MAKE = '-j 4'

DL_DIR ?= "${BSPDIR}/downloads/"

ACCEPT_FSL_EULA = ""

PREFERRED_PROVIDER_virtual/mesa = ""

DISTRO_FEATURES_remove = "x11 wayland directfb "

IMAGE_INSTALL_append = " \

qtquickcontrols-qmlplugins \

"

PACKAGECONFIG_append_pn-qtquickcontrols = " accessibility"

PACKAGECONFIG_append_pn-qtbase = " accessibility"

$ bitbake meta-toolchain-qt5

Loading cache: 100% |###########################################################################################################| ETA:  00:00:00

Loaded 2185 entries from dependency cache.

NOTE: Resolving any missing task queue dependencies

NOTE: multiple providers are available for jpeg (jpeg, libjpeg-turbo)

NOTE: consider defining a PREFERRED_PROVIDER entry to match jpeg

NOTE: multiple providers are available for runtime libgl-mesa-dev (mesa, mesa-gl)

NOTE: consider defining a PREFERRED_PROVIDER entry to match libgl-mesa-dev

NOTE: multiple providers are available for runtime libglapi (mesa, mesa-gl)

NOTE: consider defining a PREFERRED_PROVIDER entry to match libglapi

Build Configuration:

BB_VERSION        = "1.22.0"

BUILD_SYS         = "x86_64-linux"

NATIVELSBSTRING   = "Ubuntu-12.04"

TARGET_SYS        = "arm-poky-linux-gnueabi"

MACHINE           = "imx6qsabresd"

DISTRO            = "poky"

DISTRO_VERSION    = "1.6.2"

TUNE_FEATURES     = "armv7a vfp neon callconvention-hard cortexa9"

TARGET_FPU        = "vfp-neon"

meta         

meta-yocto        = "(nobranch):30b8d9378b8260e452552b806610dc9b6fe0b69f"

meta-oe           = "(nobranch):8065dd8456913457a0114ddb2b4bd4842847b2a3"

meta-fsl-arm      = "(nobranch):9bc540eec9a7e280af13371ea70650fcc47ea627"

meta-fsl-arm-extra = "(nobranch):e1085deb3d915d2a95a65cceadc77c6de0dadfb6"

meta-fsl-demos    = "(nobranch):f141c7d1158b8addbd6f1ed047a1b47c2ed85f8f"

meta-fsl-arm 

meta-fsl-demos    = "(nobranch):e6f24ebca19440924b7bf485974710ee0338ea57"

meta-browser      = "(nobranch):63963cc56c8d0291779693e62b66cb16e5c86883"

meta-gnome   

meta-networking

meta-ruby         = "(nobranch):8065dd8456913457a0114ddb2b4bd4842847b2a3"

meta-qt5          = "(nobranch):c29c317e0f22202bfaa85329a580564bbc179089"

meta-fsl-qt5 

meta-fsl-bluez    = "(nobranch):e6f24ebca19440924b7bf485974710ee0338ea57"

NOTE: Preparing runqueue

NOTE: Executing SetScene Tasks

NOTE: Executing RunQueue Tasks

WARNING: Failed to fetch URL git://qt.gitorious.org/qt/qtsystems.git;branch=dev, attempting MIRRORS if available

ERROR: Fetcher failure: Fetch command failed with exit code 128, output:

Cloning into bare repository '/home/dostojic/sabresd_yocto/downloads//git2/qt.gitorious.org.qt.qtsystems.git'...

fatal: The remote end hung up unexpectedly

ERROR: Function failed: Fetcher failure for URL: 'git://qt.gitorious.org/qt/qtsystems.git;branch=dev'. Unable to fetch URL from any source.

ERROR: Logfile of failure stored in: /home/dostojic/sabresd_yocto/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/qtsystems/5.2.1+gitAUTOINC+aa651c73bf-r0/temp/log.do_fetch.21821

ERROR: Task 814 (/home/dostojic/sabresd_yocto/sources/meta-qt5/recipes-qt/qt5/qtsystems_git.bb, do_fetch) failed with exit code '1'

NOTE: Tasks Summary: Attempted 1927 tasks of which 1917 didn't need to be rerun and 1 failed.

Waiting for 0 running tasks to finish:

Summary: 1 task failed:

  /home/dostojic/sabresd_yocto/sources/meta-qt5/recipes-qt/qt5/qtsystems_git.bb, do_fetch

Summary: There was 1 WARNING message shown.

Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

Labels (3)
1 Solution
1,465 Views
daiane_angolini
NXP Employee
NXP Employee
0 Kudos
Reply
2 Replies
1,466 Views
daiane_angolini
NXP Employee
NXP Employee

Please, repo sync

the patch was included in the tree:

meta-fsl-bsp-release.git - Freescale i.MX Yocto BSP Release Layer

0 Kudos
Reply
1,465 Views
DraganOstojic
Contributor V

Hi Daiane, this made it work.

Thanks, Dragan