bcmdhd_wlan probing fails on imx8mqevk board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

bcmdhd_wlan probing fails on imx8mqevk board

1,031 Views
ysandeepkumar07
Contributor II

Hi all,

 

I am using imx8mqevk boardv3 development board Release - Linux 4.9.88_2.0.0_ga. wireless interface is missing. So on checking dmesg, I can see that bcmdhd_wlan probing fails. see below log.

[    2.448885] bcmdhd_wlan@0 supply wlreg_on not found, using dummy regulator
[    2.449100] bcmdhd_wlan: probe of bcmdhd_wlan@0 failed with error -1

So its a pre-build, hence wifi/bt  module should be working directly, what may be the solution to start wifi and bluetooth both.

0 Kudos
2 Replies

729 Views
igorpadykov
NXP Employee
NXP Employee

Hi sandeep

currently Linux L4.9.51 is "GA" officially supported release for i.MX8M and

supports QCA6174A, its usage can be found in documentation below

https://www.nxp.com/webapp/Download?colCode=L4.9.51_8MQ_GA_LINUX_DOCS&Parent_nodeId=1337699481071706... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

729 Views
ysandeepkumar07
Contributor II

Actually we are planning to use Release - Linux 4.9.88_2.0.0_ga only for our custom board development. So may I know, how can we support QCA6174 for this release. Or may I know when will NXP officially releases 4.9.88_2.0.0_ga with full working stack.

0 Kudos