audio source codes support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

audio source codes support

跳至解决方案
4,167 次查看
dongyang12
Contributor I

I would like to port our internal voice algorithm into i.MX 8MM, but I needs some audio source code from SoC chip which including each microphone raw and AEC reference signals, as well as transport Tx signal via USB. There have some detail demand.

The sample rate can support 16K and 24K.

Support dump original microphone signal and AEC reference signal data together.

The delay between microphone signal and reference signal is stable.

 

At currently stage, I will use IMX 8MM as a USB device.

There need two audio input sources.

Microphone input : Audio from digital microphones. (4 microphones)

Rx input: Audio from the far-end device. For example, receive the audio signal via USB.

 

There need two audio output sources.

RX out: Processed audio(just bypass) to play in the near-end device speaker.

TX out: Processed audio(just bypass) to send back the far-end device. For example, transport the signal to far-end device via USB.

 

 

标签 (1)
0 项奖励
回复
1 解答
3,984 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

If you have extracted the toolchain from Yocto it should be correct. You can generate a .sh to install the toolchain using Yocto with the following command:

$ bitbake imx-image-multimedia -c populate_sdk

The default path for installing the toolchain is /opt, your toolchain should have the asound header on a couple of paths. If this is not available there may be a problem with the toolchain.

/opt/<DISTRO>/<BSP>/sysroots/armv8a-poky-linux/usr/include/sys/asoundlib.h
/opt/<DISTRO>/<BSP>/sysroots/armv8a-poky-linux/usr/include/asoundlib.h
/opt/<DISTRO>/<BSP>/sysroots/armv8a-poky-linux/usr/include/alsa/asoundlib.h

As for the Real Time Edge image, it does not include the AFE so you would need to install it manually. You may copy the files from /unit_tests/nxp-afe and /usr/lib/nxp-afe/ to the same paths on the Real Time Edge image to run the AFE.

The asound.conf file ready to be used with the AFE is available in /unit_tests/nxp-afe/asound.conf

For the i.MX8MM you may use the default asound.conf available in this directory. There are separate configurations for other boards or configurations.

I hope that this information helps.

 

在原帖中查看解决方案

0 项奖励
回复
5 回复数
4,099 次查看
dongyang12
Contributor I

Hello,

Thanks your detialed information, and I found some problems during experiment. There have four questions, could you help me check it?

1, it will happen error when I build https://github.com/nxp-imx/nxp-afe. It can't found alsa/asoundlib.h, Could you help check it?

nxp_afe_build_error.PNG

2, The AFE is already integrated on the i.MX Linux BSP. Do you mean file "nxp-afe_git.bb" in the folder meta-imx/meta-bsp/recipes-multimedia/nxp-afe? 

3, Because I can't build success by make with source code. So I try to build it using bitbake nxp-afe in the yocto and generate a package. And I install this package in the IMX8MM board. And I do test according to the file "/unit_tests/nxp-afe/TODO.md". It can work and I can hear the sound from the headphone. But the output file from record only have 1 channel, and it didn't include reference signal. How to setup AFE if I need 4 channel mic signal and 1 channel reference?

4, Running the script UAC_VCOM_composite.sh after connect the board to Windows PC. The PC can recognized sink/mic card. But the board no sound output when I play music in PC. And the PC can't capture the data when I start record. 

0 项奖励
回复
4,091 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi,

0 项奖励
回复
4,031 次查看
dongyang12
Contributor I
Hi,
Thanks your information. And I have some question need your support.
1), My toolchain is get from the folder build_folder/tmp/deploy/sdk/ after build the yocto sdk successfully. Is it different with what you said. Could you tell me how to extract the toolchain from the Yocto BSP and use it to build the AFE. Because using bitbake nxp-afe build the AFE, it will use the default setup and I can't change the setup and code.
2), I download the image "Real-time_Edge_v2.5_IMX8MM-LPDDR4-EVK.zip" from official website. But it doesn't install the AFE in path /unit_test/nxp-afe. Could you provide the link the demo image to me?
3) I will confirm and check it.
4) Do you mean that I need to change the configure file asound.conf? Could you give a example to me?
0 项奖励
回复
3,985 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

If you have extracted the toolchain from Yocto it should be correct. You can generate a .sh to install the toolchain using Yocto with the following command:

$ bitbake imx-image-multimedia -c populate_sdk

The default path for installing the toolchain is /opt, your toolchain should have the asound header on a couple of paths. If this is not available there may be a problem with the toolchain.

/opt/<DISTRO>/<BSP>/sysroots/armv8a-poky-linux/usr/include/sys/asoundlib.h
/opt/<DISTRO>/<BSP>/sysroots/armv8a-poky-linux/usr/include/asoundlib.h
/opt/<DISTRO>/<BSP>/sysroots/armv8a-poky-linux/usr/include/alsa/asoundlib.h

As for the Real Time Edge image, it does not include the AFE so you would need to install it manually. You may copy the files from /unit_tests/nxp-afe and /usr/lib/nxp-afe/ to the same paths on the Real Time Edge image to run the AFE.

The asound.conf file ready to be used with the AFE is available in /unit_tests/nxp-afe/asound.conf

For the i.MX8MM you may use the default asound.conf available in this directory. There are separate configurations for other boards or configurations.

I hope that this information helps.

 

0 项奖励
回复
4,129 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You may find NXP’s Audio Front End (AFE) useful, which allows to load signal processors from different vendors and configure all the necessary streams to make the whole chain functional. You can find more information in section 8.3.3 of the i.MX Linux User’s Guide (link below). You can setup the AFE to your needs (TX and RX streams, number of microphones, etc).

https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf

The repository for the AFE can be found on the link below. The AFE is already integrated on the i.MX Linux BSP.

https://github.com/nxp-imx/nxp-afe

Please note that stability of the delay between the microphone signal and reference signal would be dependent on the audio chain setup and the load of the Linux system, as interruptions from other services may affect this delay.

As for an USB solution to transport the audio streams, one alternative is using an USB composite gadget as to allow input and output streams. You can find an example attached that creates a USB Composite using the Serial Gadget (g_serial) and an UAC Gadget (g_audio) drivers already in Linux. Please note that an UDC must be available to run the script, so please connect the board to a Windows or Linux host before running the script.

I hope this information helps!

 

0 项奖励
回复