Hello,
I've a i.MX6Quad and wm8960 codec and i'm trying to run this setup.
I've seen wm8962 and sgtl5000 files, but many things are not clear for me.
Can someone explain me in an approachable way how to write an audio codec driver or where to gain knowledge about this subject?
Regards,
Sebastian B.
Original Attachment has been moved to: imx6qdl.dtsi.zip
Original Attachment has been moved to: imx6qdl-sabresd.dtsi.zip
Original Attachment has been moved to: imx-wm8960.c.zip
You can use the imx_3.14.28_7d_alpha branch. In imx7d-sdb board there is a wm8960 codec:
linux-2.6-imx.git - Freescale i.MX Linux Tree
,so you can use this as a reference and modify your dts accordingly.
Regards,
Fabio Estevam
Hi Fabio:
I prot the driver from imx_3.14.28_7d_alpha branch to andorid4.4.3 imx6q,only modify the dts,as follow:
reg_audio: wm8960_supply {
compatible = "regulator-fixed";
regulator-name = "wm8960-supply";
gpio = <&gpio4 23 0>;
enable-active-high;
};
sound {
compatible = "fsl,imx6q-sabresd-wm8960",
"fsl,imx-audio-wm8960";
model = "wm8960-audio";
cpu-dai = <&ssi2>;
audio-codec = <&codec>;
codec-master;
};
codec: wm8960@1a {
compatible = "wlf,wm8960";
reg = <0x1a>;
clocks = <&clks 201>;
clock-names = "mclk";
wlf,shared-lrclk;
};
The sound’s card has been found.But can't play music.
When i use the tiny tool,it show below
root@sabresd_6dq:/sdcard/Music # tinyplay xiaopinguo.wav
ASoC: HiFi startup failed: -16
cannot open device '/dev/snd/pcmC0D0p'
Unable to open PCM device 0.
can you help me to analyze what the problems.
The dts and log pls reference to the attachment.
Thanks
Hi Nikolaenko,
Thank you so much for your immediate reply.
Actually we are using SGTL5000 codec(with internal clock).
I will check the differences you have done for wm8960 and implement the same changes for SGTL5000.
Best Regards,
Lakshmi Hegde
Hi Sebastian!
Could you share your imx-wm8960 driver and .dts file nodes with the community, please?
I have my own wm8960 driver, but it is not able to capture sound from microphone.
Thank You.
Hi Sebastian
some descriptions can be found in attached Porting Guide
sect.Chapter 8 Porting Audio Codecs to a Custom Board,
MX53UG Chapter 21 Porting Audio Codecs to a Custom Board,
Chapter 29 Advanced Linux Sound Architecture (ALSA) System
on a Chip (ASoC) Sound Driver Linux Manual
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I somehow clicked as resolved:( Can admin please revert it?
Thank You Igor for the answer.
I already read porting guide.
Now i'm receiving this error
imx-wm8960 sound.22: ASoC: CODEC DAI wm8960 not registered
imx-wm8960 sound.22: snd_soc_register_card failed (-517)
Can You give me some hints?
Regards,
Sebastian
Hi Igor,
I couldn't answer before the weekend.
I2C is working, i have signals on the lines, i checked it with other custom device and it's sending what i want.
I have checked wm8960.c file and found that function "wm8960_i2c_probe" is performed and no function returns error.
Also i2c device is registered.
In this file there is also "wm8960_probe" function but it's not running.
Unfortunately WM8960 is write only device, and i cannot read its registers:/
Hi Sebastian
Linux/Documentation/devicetree/bindings/sound/wm8960.txt - Linux Cross Reference - Free Electrons
linuxppc-dev - [alsa-devel][PATCH] ASoC: fsl: add imx-wm8960 machine driver
Advanced Linux Sound System development
if you have Sabre SD board (it supports wm8962 codec)
then one can run both boards in parallel and with debugger run
program step by step. So one can find where custom board fails from
normal flow execution. Recommended to use Freescale BSP from
official product web page
L3.14.28_1.0.0_iMX6QDLS_BUNDLE
AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors
Also Freescale has special service for providing support for customization
of drivers which are not present on its BSP releases:
Professional Engineering Services|Freescale
Best regards
igor