ask for audio and audio card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ask for audio and audio card

836 Views
qiaoweibiao
Contributor III

   I want to know the different of performance bettween SAI1 and SAI3.

As i know the SAI1 from M4 and SAI3 from A53.So can I use the SAI3 to send the music to the audio card? Thanks a lot!

Labels (2)
Tags (1)
4 Replies

730 Views
qiaoweibiao
Contributor III

或者我这样问 SAI3 是否支持DSD512 谢谢 

0 Kudos

730 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

For which i.MX are you talking for?

Best regards,

Diego.

0 Kudos

730 Views
qiaoweibiao
Contributor III

Hi ,

I  want to know that about IMX8M mini.

1.I see the SAI1(3.3V ) also used for boot CFG .If i change the  power of SAI1(3.3V )  to  SAI1(1.8V) ,also to every part about SAI1.

Does the boot CFG work normal  ? As i need use the SAI1 works at the level of 1.8V  ranther than 3.3V.

thanks a lot !

0 Kudos

730 Views
diegoadrian
NXP Employee
NXP Employee

According to the i.MX8MM datasheet. There is no problem if you use 1.8 to supply the SAI1. It supports voltages from 0V to 3.8V

sai voltages.jpg

Best regards,

Diego.