arm-smmu 51400000.iommu: Unhandled context fault: fsr=0x402, iova=0xfe27a000, fsynr=0x100013, cb=0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

arm-smmu 51400000.iommu: Unhandled context fault: fsr=0x402, iova=0xfe27a000, fsynr=0x100013, cb=0

2,768 Views
vinothkumars
Senior Contributor IV

Hi All,

 

I got kernel crash, I don't know what exactly, Will you please give me some ideas

 

mek_8q:/ $
[ 4.348072] ++++++++++++++ arm_smmu_context_fault ++++++++++++ interrupt: 12
[ 4.348124] +++++++ Unable to handle kernel paging request at virtual address ffffbb884fc3d000
[ 4.350649] ------------[ cut here ]------------
[ 4.350673] WARNING: CPU: 1 PID: 1138 at /home/emb-vinosek/Documents/VINOTH/IndiEV-IMX8-A9/source/vendor/nxp-opensource/kernel_imx/drivers/iommu/io-pgtable-arm.c:305 __arm_lpae_map+0x17c/0x318

 

.356243] [<ffff00000852caf0>] __arm_lpae_map+0x160/0x318
[ 4.356247] [<ffff00000852ca9c>] __arm_lpae_map+0x10c/0x318
[ 4.356251] [<ffff00000852ca9c>] __arm_lpae_map+0x10c/0x318
[ 4.356255] [<ffff00000852ca9c>] __arm_lpae_map+0x10c/0x318
[ 4.356259] [<ffff00000852cd74>] arm_lpae_map+0xcc/0x100
[ 4.356263] [<ffff00000852ee04>] arm_smmu_map+0x18/0x28
[ 4.356267] [<ffff0000085282e0>] iommu_map+0xc0/0x248
[ 4.356271] [<ffff00000852856c>] default_iommu_map_sg+0x104/0x16c
[ 4.356275] [<ffff00000852b318>] iommu_dma_map_sg+0x148/0x2fc
[ 4.356280] [<ffff00000809bbd4>] __iommu_map_sg_attrs+0x6c/0x7c
[ 4.356287] [<ffff0000086e5540>] cqhci_request+0x194/0x4e8
[ 4.356292] [<ffff0000086c2418>] mmc_cqe_start_req+0x58/0x108
[ 4.356296] [<ffff0000086d60ac>] mmc_blk_mq_issue_rq+0x2d4/0x3ac
[ 4.356300] [<ffff0000086d6aa8>] mmc_mq_queue_rq+0x134/0x27c
[ 4.356304] [<ffff0000083ddb48>] blk_mq_dispatch_rq_list+0x354/0x42c
[ 4.356310] [<ffff0000083e21f4>] blk_mq_sched_dispatch_requests+0x174/0x200
[ 4.356313] [<ffff0000083dbd68>] __blk_mq_run_hw_queue+0x9c/0x108
[ 4.356317] [<ffff0000083dbe24>] blk_mq_run_work_fn+0x50/0x64
[ 4.356322] [<ffff0000080cb990>] process_one_work+0x140/0x3f8
[ 4.356326] [<ffff0000080cbd80>] worker_thread+0x138/0x3e4
[ 4.356331] [<ffff0000080d1d68>] kthread+0x104/0x130
[ 4.356336] [<ffff000008084f14>] ret_from_fork+0x10/0x18

 

 

Regards,
Vinothkumar Sekar
0 Kudos
1 Reply

2,750 Views
jamesbone
NXP TechSupport
NXP TechSupport

Virtual addressing works by indirect addressing. There is a page table which indicates where that page is in real memory and the hardware uses the page table to indirectly address memory. Until the kernel gets the page table set up it runs in real mode where it uses the real address of memory locations.

So I read your symptoms and thought that maybe the kernel and the hardware disagreed on how to handle virtual memory, i.e. the kernel was compiled for the wrong cpu, or you do not have enough memory or not accesible.

 

0 Kudos