are there any linux audio encoders available that will take input from the i.mx28 lrad iio interface?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

are there any linux audio encoders available that will take input from the i.mx28 lrad iio interface?

ソリューションへジャンプ
1,419件の閲覧回数
tylerarnold
Contributor II

I am trying to encode audio , or at least for now sample PCM audio from the LRAD Channel 0 interface, using the mxs-lradc driver and the iio interface.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,350件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Tyler

I am afraid there is no such encoder.

Also since in Linux it is not possible to have accurate sample timings with

LRADC usage, such driver would not be useful.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,351件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Tyler

I am afraid there is no such encoder.

Also since in Linux it is not possible to have accurate sample timings with

LRADC usage, such driver would not be useful.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,350件の閲覧回数
tylerarnold
Contributor II

bummer.

0 件の賞賛
返信