any region for OEM key in Imx6q sbrelite board?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

any region for OEM key in Imx6q sbrelite board?

496件の閲覧回数
myungjinhwang
Contributor III

dear freescale team.

question...

any region for OEM key in Imx6q sbrelite board like OCOTP or others?

except for OCOTP_SRK[0~255].

there are shadow registers of the 4Kbit OCOTP.

all the shadow registers are assigned for some purpose?

please let me know if there are  regions on the board for R/W of OEM key.

best regards

myungjin hwang

0 件の賞賛
3 返答(返信)

374件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi MyungJin

fuses which can be used for customer purposes one can find

in Table 5-10. Fusemap Descriptions i.MX6DQ Reference Manual (rev.3  7/2015)

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

374件の閲覧回数
myungjinhwang
Contributor III

could you explain it more in detailed?

you mean OCOTP_SRK[0~255] or GP1, GP2?

i mentioned except for OCOTP_SRK[0~255].

Best regards

myungjin hwang

0 件の賞賛

374件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

one can use any fuses marked "Customer / OEM use"

for own purposes.

Best regards

igor

0 件の賞賛