any region for OEM key in Imx6q sbrelite board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

any region for OEM key in Imx6q sbrelite board?

498 Views
myungjinhwang
Contributor III

dear freescale team.

question...

any region for OEM key in Imx6q sbrelite board like OCOTP or others?

except for OCOTP_SRK[0~255].

there are shadow registers of the 4Kbit OCOTP.

all the shadow registers are assigned for some purpose?

please let me know if there are  regions on the board for R/W of OEM key.

best regards

myungjin hwang

0 Kudos
3 Replies

376 Views
igorpadykov
NXP Employee
NXP Employee

Hi MyungJin

fuses which can be used for customer purposes one can find

in Table 5-10. Fusemap Descriptions i.MX6DQ Reference Manual (rev.3  7/2015)

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

376 Views
myungjinhwang
Contributor III

could you explain it more in detailed?

you mean OCOTP_SRK[0~255] or GP1, GP2?

i mentioned except for OCOTP_SRK[0~255].

Best regards

myungjin hwang

0 Kudos

376 Views
igorpadykov
NXP Employee
NXP Employee

one can use any fuses marked "Customer / OEM use"

for own purposes.

Best regards

igor

0 Kudos