android8.0 porting on IMX8MQ EVK board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

android8.0 porting on IMX8MQ EVK board

183件の閲覧回数
prasanth
Contributor I

Hi,

We are porting Android8.0 operating system in Imx8mq evk board. We are using below link to download the source and getting below error. Please help me to resolve the below error.

Used link:

 repo init -u https://source.codeaurora.org/external/imx/imx-manifest.git -b imx-android-oreo -m imx-o8.0.0_1.3.0_8mq-prc.xml

Error:

fatal: Unable to look up git.freescale.com (port 9418) (Name or service not known)

imx-firmware:
fatal: Unable to look up git.freescale.com (port 9418) (Name or service not known)
imx-firmware: sleeping 4.0 seconds before retrying
fatal: Unable to look up git.freescale.com (port 9418) (Name or service not known)

imx-firmware:
fatal: Unable to look up git.freescale.com (port 9418) (Name or service not known)
error: Cannot fetch imx-firmware from git://git.freescale.com/proprietary/imx-firmware
Fetching: 100% (598/598), done in 1m30.050s
Garbage collecting: 100% (598/598), done in 1.241s

fatal: Unable to look up git.freescale.com (port 9418) (Name or service not known)

imx-firmware:
fatal: Unable to look up git.freescale.com (port 9418) (Name or service not known)
imx-firmware: sleeping 4.0 seconds before retrying
fatal: Unable to look up git.freescale.com (port 9418) (Name or service not known)

imx-firmware:
fatal: Unable to look up git.freescale.com (port 9418) (Name or service not known)
error: Cannot fetch imx-firmware from git://git.freescale.com/proprietary/imx-firmware
Fetching: 100% (1/1), done in 4.019s
Garbage collecting: 100% (1/1), done in 0.004s
Checking out: 100% (598/598), done in 6.653s

error: Unable to fully sync the tree.
error: Downloading network changes failed.
Try re-running with "-j1 --fail-fast" to exit at the first error.

 

Thanks,

Prasanth

0 件の賞賛
0 返答(返信)