android8.0 porting on IMX8MQ EVK board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

android8.0 porting on IMX8MQ EVK board

198 次查看
prasanth
Contributor I

Hi,

We are porting Android8.0 operating system in Imx8mq evk board. We are using below link to download the source and getting below error. Please help me to resolve the below error.

Used link:

 repo init -u https://source.codeaurora.org/external/imx/imx-manifest.git -b imx-android-oreo -m imx-o8.0.0_1.3.0_8mq-prc.xml

Error:

fatal: Unable to look up git.freescale.com (port 9418) (Name or service not known)

imx-firmware:
fatal: Unable to look up git.freescale.com (port 9418) (Name or service not known)
imx-firmware: sleeping 4.0 seconds before retrying
fatal: Unable to look up git.freescale.com (port 9418) (Name or service not known)

imx-firmware:
fatal: Unable to look up git.freescale.com (port 9418) (Name or service not known)
error: Cannot fetch imx-firmware from git://git.freescale.com/proprietary/imx-firmware
Fetching: 100% (598/598), done in 1m30.050s
Garbage collecting: 100% (598/598), done in 1.241s

fatal: Unable to look up git.freescale.com (port 9418) (Name or service not known)

imx-firmware:
fatal: Unable to look up git.freescale.com (port 9418) (Name or service not known)
imx-firmware: sleeping 4.0 seconds before retrying
fatal: Unable to look up git.freescale.com (port 9418) (Name or service not known)

imx-firmware:
fatal: Unable to look up git.freescale.com (port 9418) (Name or service not known)
error: Cannot fetch imx-firmware from git://git.freescale.com/proprietary/imx-firmware
Fetching: 100% (1/1), done in 4.019s
Garbage collecting: 100% (1/1), done in 0.004s
Checking out: 100% (598/598), done in 6.653s

error: Unable to fully sync the tree.
error: Downloading network changes failed.
Try re-running with "-j1 --fail-fast" to exit at the first error.

 

Thanks,

Prasanth

0 项奖励
0 回复数