android6.0 mfgtools android_m6.0.1_2.0.0_ga_tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

android6.0 mfgtools android_m6.0.1_2.0.0_ga_tool

1,778件の閲覧回数
baozhuliu
Contributor III

Android6.0烧写出错,mfgtools工具从Jumping to OS image跳到No Device Connected,然后一直卡在No Device Connected,串口信息如下:

U-Boot 2015.04-14490-g596b7a8-dirty (Nov 15 2016 - 11:55:26)

CPU: Freescale i.MX6D rev1.5 at 792 MHz
CPU: Temperature 31 C
Reset cause: POR
Board: MX6-SabreSD
I2C: ready
DRAM: 1 GiB
1111Bus: 0 PMIC:PFUZE100 probed!
PMIC: PFUZE100 ID=0x10
MMC:
FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2

*** Warning - bad CRC, using default environment

No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
check_and_clean: reg 0, flag_set 0
Fastboot: Normal
flash target is MMC:2
Net: FEC [PRIME]
Error: FEC address not set.

Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: <NULL>
=>

一直卡在这,使用的是android_m6.0.1_2.0.0_ga_tool烧写的。还请专业人员给点建议

ラベル(5)
0 件の賞賛
返信
4 返答(返信)

1,342件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi baozhu,

Which board are you using? Here which device do you want to falsh, emmc or SD card?
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,342件の閲覧回数
baozhuliu
Contributor III

Hi Rita

1.board:  MX6Q SABRESD

2.Device which I you want to falsh :  emmc

I hope you can give some advice.  Thank you!

0 件の賞賛
返信

1,342件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi baozhu,

The images you flash to emmc are the demo images you download from our website or you build yourself?

I will try it on my board later and give you detail reply.

Have a great day,
Rita

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,342件の閲覧回数
baozhuliu
Contributor III

We are now using the board will be the original board of the PMIC connection to the seat changed.So the images I flash to emmc are the  I build myself.

0 件の賞賛
返信