Android6.0烧写出错,mfgtools工具从Jumping to OS image跳到No Device Connected,然后一直卡在No Device Connected,串口信息如下:
U-Boot 2015.04-14490-g596b7a8-dirty (Nov 15 2016 - 11:55:26)
CPU: Freescale i.MX6D rev1.5 at 792 MHz
CPU: Temperature 31 C
Reset cause: POR
Board: MX6-SabreSD
I2C: ready
DRAM: 1 GiB
1111Bus: 0 PMIC:PFUZE100 probed!
PMIC: PFUZE100 ID=0x10
MMC:
FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
check_and_clean: reg 0, flag_set 0
Fastboot: Normal
flash target is MMC:2
Net: FEC [PRIME]
Error: FEC address not set.
Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: <NULL>
=>
一直卡在这,使用的是android_m6.0.1_2.0.0_ga_tool烧写的。还请专业人员给点建议
Hi baozhu,
Which board are you using? Here which device do you want to falsh, emmc or SD card?
Have a great day,
Rita
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Rita
1.board: MX6Q SABRESD
2.Device which I you want to falsh : emmc
I hope you can give some advice. Thank you!
Hi baozhu,
The images you flash to emmc are the demo images you download from our website or you build yourself?
I will try it on my board later and give you detail reply.
Have a great day,
Rita
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
We are now using the board will be the original board of the PMIC connection to the seat changed.So the images I flash to emmc are the I build myself.