I'm working with an iMX6 SabreSD board. I've got the board booting from eMMC. I have been able to build the kernel Image and android image and can flash the board using the MfgTool successfully.
I am currently trying to set up my development environment to have android boot up over NFS and kernel over TFTP. My host machine runs Ubuntu 12.04.
I've followed the instructions in the i.MX_Android_R13.3_User_Guide.html document that came with the imx-android-r13.3 package for the build and setting up of the nfs directory.
The kernel comes up correctly, but I am having problems with the NFS boot part. (Kernel's uImage is available in /var/lib/tftpboot/)
Output of /etc/exports:
/var/lib/export-rfs *(rw,no_root_squash,async,no_subtree_check)
The android rootfs is available under /var/lib/export-rfs/sabresd_6q
After copying over the files to /var/lib/export-rfs/sabresd_6q, I modified init.freescale.rc and commented out the lines that would mount /system /data/, etc from /dev/block/mmcblk0p*.
I can mount the nfs directory on a pc correctly and have no read-write issues. NFS works ok otherwise. I am using it successfully for other directories under /var/lib/export-rfs on different machines.
The output on the console from the boot up sequence is attached.
The logcat output shows the following errors :
I/dalvikvm( 3987): Unable to open or create cache for /system/framework/core.jar (/data/dalvik-cache/system@framework@core.jar@classes.dex)
D/dalvikvm( 3987): Unable to process classpath element '/system/framework/core.jar'
E/dalvikvm( 3987): Could not stat dex cache directory '/data/dalvik-cache': No such file or directory
I/dalvikvm( 3987): Unable to open or create cache for /system/framework/core-junit.jar (/data/dalvik-cache/system@framework@core-junit.jar@classes.dex)
D/dalvikvm( 3987): Unable to process classpath element '/system/framework/core-junit.jar'
E/dalvikvm( 3987): Could not stat dex cache directory '/data/dalvik-cache': No such file or directory
I/dalvikvm( 3987): Unable to open or create cache for /system/framework/bouncycastle.jar (/data/dalvik-cache/system@framework@bouncycastle.jar@classes.dex)
D/dalvikvm( 3987): Unable to process classpath element '/system/framework/bouncycastle.jar'
E/dalvikvm( 3987): Could not stat dex cache directory '/data/dalvik-cache': No such file or directory
I/dalvikvm( 3987): Unable to open or create cache for /system/framework/ext.jar (/data/dalvik-cache/system@framework@ext.jar@classes.dex)
D/dalvikvm( 3987): Unable to process classpath element '/system/framework/ext.jar'
E/dalvikvm( 3987): Could not stat dex cache directory '/data/dalvik-cache': No such file or directory
I/dalvikvm( 3987): Unable to open or create cache for /system/framework/framework.jar (/data/dalvik-cache/system@framework@framework.jar@classes.dex)
D/dalvikvm( 3987): Unable to process classpath element '/system/framework/framework.jar'
E/dalvikvm( 3987): Could not stat dex cache directory '/data/dalvik-cache': No such file or directory
I/dalvikvm( 3987): Unable to open or create cache for /system/framework/android.policy.jar (/data/dalvik-cache/system@framework@android.policy.jar@classes.dex)
D/dalvikvm( 3987): Unable to process classpath element '/system/framework/android.policy.jar'
E/dalvikvm( 3987): Could not stat dex cache directory '/data/dalvik-cache': No such file or directory
I/dalvikvm( 3987): Unable to open or create cache for /system/framework/services.jar (/data/dalvik-cache/system@framework@services.jar@classes.dex)
D/dalvikvm( 3987): Unable to process classpath element '/system/framework/services.jar'
E/dalvikvm( 3987): Could not stat dex cache directory '/data/dalvik-cache': No such file or directory
I/dalvikvm( 3987): Unable to open or create cache for /system/framework/apache-xml.jar (/data/dalvik-cache/system@framework@apache-xml.jar@classes.dex)
D/dalvikvm( 3987): Unable to process classpath element '/system/framework/apache-xml.jar'
E/dalvikvm( 3987): Could not stat dex cache directory '/data/dalvik-cache': No such file or directory
I/dalvikvm( 3987): Unable to open or create cache for /system/framework/filterfw.jar (/data/dalvik-cache/system@framework@filterfw.jar@classes.dex)
D/dalvikvm( 3987): Unable to process classpath element '/system/framework/filterfw.jar'
E/dalvikvm( 3987): No valid entries found in bootclasspath '/system/framework/core.jar:/system/framework/core-junit.jar:/system/framework/bouncycastle.jar:/system/framework/ext.jar:/system/framework/framework.jar:/system/framework/android.policy.jar:/system/framework/services.jar:/system/framework/apache-xml.jar:/system/framework/filterfw.jar'
E/dalvikvm( 3987): VM aborting
F/libc ( 3987): Fatal signal 11 (SIGSEGV) at 0xdeadd00d (code=1)
So it looks like it can't access /system and /data, etc.
The files are available as read-only when I do an ls -l on the target. (Can't write to them). I can't do a touch successfully.
Running mount shows the following output:
192.168.1.112:/var/lib/export-rfs/sabresd_6q/ / nfs ro,relatime,vers=3,rsize=4096,wsize=4096,namlen=255,hard,nolock,proto=tcp,timeo=600,retrans=2,sec=sys,mountaddr=192.168.1.112,mountvers=3,mountproto=tcp,local_lock=all,addr=192.168.1.112 0 0
tmpfs /dev tmpfs rw,nosuid,relatime,mode=755 0 0
devpts /dev/pts devpts rw,relatime,mode=600 0 0
proc /proc proc rw,relatime 0 0
sysfs /sys sysfs rw,relatime 0 0
none /acct cgroup rw,relatime,cpuacct 0 0
tmpfs /mnt/asec tmpfs rw,relatime,mode=755,gid=1000 0 0
tmpfs /mnt/obb tmpfs rw,relatime,mode=755,gid=1000 0 0
tmpfs /mnt/shm tmpfs rw,relatime,size=1024k,mode=775,uid=1000,gid=1003 0 0
none /dev/cpuctl cgroup rw,relatime,cpu 0 0
none /sys/kernel/debug debugfs rw,relatime 0 0
root@android:/ #
The output of Uboot environemt:
bootdelay=3
baudrate=115200
netmask=255.255.255.0
rd_loadaddr=0x11000000
netdev=eth0
ethprime=FEC0
fastboot_dev=mmc3
ethact=FEC0
ipaddr=192.168.1.103
loadaddr=0x10800000
bootfile=uImage
serverip=192.168.1.112
nfsroot=var/lib/export-rfs/sabresd_6q
bootcmd=dhcp;bootm
stdin=serial
stdout=serial
stderr=serial
bootargs=console=ttymxc0,115200 init=/init rw video=mxcfb0 ip=dhcp fbmem=10M nfsroot=192.168.1.112:/var/lib/export-rfs/sabresd_6q vmalloc=400M androidboot.console=ttymxc0
Environment size: 509/8188 bytes
MX6Q SABRESD U-Boot >
This is what I set it as in U-Boot:
setenv bootargs console=ttymxc0,115200 init=/init rw video=mxcfb0 ip=dhcp fbmem=10M nfsroot=${serverip}:/${nfsroot}, vmalloc=400M androidboot.console=ttymxc0
The bootargs variable for the console is specifying it as rw, but it looks like / is finally mounted as ro. Any ideas on where I can change this or what can be causing these errors.
Thanks.
Regards,
-Rema.
Original Attachment has been moved to: bootconsole.txt.zip
已解决! 转到解答。
Thanks Daiane.
After a bit of trial and error after I had posted this problem, I discovered that adding the mount with the nfs command in the init.freescale.rc file had fixed this issue.
Hi Reema,
I am also getting the same issue while encrypting/decrypting the phone and after encryption is done when device is trying to reboot i am getting this issue,so there is something i need to modify in the init files.
Can u please tell what exactly you have changed to resolve this issue.
Thanks,
Durgesh
My problem was that the file
./system/core/rootdir/init.rc
<snip>
on post-fs
# once everything is setup, no need to modify /
# mount rootfs rootfs / ro remount
Thinking .system/core/rootdir/init.rc ended up in the root directory of the nfs mount. Apparently it does not. I have not found the actual file that the build uses.
We also had to change
./device/fsl/imx6/sabresd/init.rc
to remove all the ext4 mounts
in the file device/fsl//imx6/sabresd/init.rc,
add a line so it doesn't try to reDHCP during boot
and comment out the ext4 mounts
setprop ethernet.clear.ip no
#on fs
# mount ext4 partitions
# mount ext4 /dev/block/mmcblk0p5 /system
# mount ext4 /dev/block/mmcblk0p5 /system ro remount
# mount ext4 /dev/block/mmcblk0p7 /data nosuid nodev nodiratime noatime
errors=panic,discard,nomblk_io_submit,noauto_da_alloc
# mount ext4 /dev/block/mmcblk0p6 /cache nosuid nodev
# mount ext4 /dev/block/mmcblk0p8 /device ro nosuid nodev