Hi,
In the user guide of android_L5.1.1_2.1.0, it is not mentioned which build should used for i.MX 6 Dual Plus, is it sabresd_6dq-user?
Thank you.
bsp is built for board, not based on chip, what board do you use? if your customized board is based on i.MX 6QuadPlus AI board, you can use this vesrion, refer to the release note, 5.1.1_2.1.0 supports i.MX 6QuadPlus SABRE-AI board and platform
Hi,
Thanks for the reply.
In the user guide, it mentioned i.MX device lunch examples:
i.MX 6Quad/DualLite SABRE-SD Board and Platform $ lunch sabresd_6dq-user
i.MX 6Quad/DualLite/QuadPlus SABRE-AI Board $ lunch sabreauto_6dq-user
So I can assume this also applies for i.MX 6 Dual Plus?
as I mentioned before, what board do you use? if your cusomized board is designed based on imx6qp sabr-AI board, you can use $ lunch sabreauto_6dq-user