amd-gpu-bin-mx51-10.11.01-1 fails to build

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

amd-gpu-bin-mx51-10.11.01-1 fails to build

1,060件の閲覧回数
KrishnaPavan
Contributor II

amd-gpu-bin-mx51-10.11.01-1

Ubuntu 10.04, ltib 9.1.1, i.MX51_EVK

Trying to build Qt!

Following Instructions from http://www.imxdev.org/wiki/index.php?title=All_Boards_Qt

Error Log:

Processing: amd-gpu-bin-mx51
==============================
sudo /opt/freescale/ltib/usr/bin/rpm --root /home/krishna/ltib/rootfs --dbpath /var/lib/rpm -e --allmatches --nodeps --define '_tmppath /tmp/ltib' amd-gpu-bin-mx51 2>/dev/null
sudo /opt/freescale/ltib/usr/bin/rpm --root /home/krishna/ltib/rootfs --dbpath /var/lib/rpm --prefix / --ignorearch -ivh --force --excludedocs --define '_tmppath /tmp/ltib' /home/krishna/ltib/rpm/RPMS/arm/amd-gpu-bin-mx51-10.11.01-1.arm.rpm
error: failed dependencies:
    libc.so.6(GLIBC_2.11)   is needed by amd-gpu-bin-mx51-10.11.01-1

f_buildrpms() returned an error, exiting
traceback:
 main:560

Started: Wed Dec 14 17:33:46 2011
Ended:   Wed Dec 14 17:35:52 2011
Elapsed: 126 seconds

Build Failed
Exiting on error or interrupt

*****************************CHECK FOR (soname) RESULTED IN************************************

 ldd -v /bin/sh
    linux-vdso.so.1 =>  (0x00007fffeb9f1000)
    libc.so.6 => /lib/libc.so.6 (0x00007f47a95d2000)
    /lib64/ld-linux-x86-64.so.2 (0x00007f47a9969000)

    Version information:
    /bin/sh:
        libc.so.6 (GLIBC_2.4) => /lib/libc.so.6
        libc.so.6 (GLIBC_2.3) => /lib/libc.so.6
        libc.so.6 (GLIBC_2.3.4) => /lib/libc.so.6
        libc.so.6 (GLIBC_2.11) => /lib/libc.so.6
        libc.so.6 (GLIBC_2.2.5) => /lib/libc.so.6
    /lib/libc.so.6:
        ld-linux-x86-64.so.2 (GLIBC_PRIVATE) => /lib64/ld-linux-x86-64.so.2
        ld-linux-x86-64.so.2 (GLIBC_2.3) => /lib64/ld-linux-x86-64.so.2

Please kindly suggest!

タグ(2)
0 件の賞賛
返信
1 返信

822件の閲覧回数
KrishnaPavan
Contributor II

Hi,

No solution has been found yet. I came to know from many forums that it might be because of the Graphic Libraries Anomaly. So, I am still looking for a solution, WRT the L2.6.35_10.11.01_ER_source bundle.

Since I was not able to make that work as per my requirements, I used a different source bundle L2.6.31_10.07.11_ER_source, and this worked.

This might be considered as to why it did happen like that? Looking forward to know reasons, If any one could suggest!

Regards  :::   Krishna Pavan

0 件の賞賛
返信