$bitbake agl-demo-platform
ERROR: psplash-0.1+gitAUTOINC+2015f7073e-r15 do_package: QA Issue: psplash: Files/directories were installed but not shipped in any package:
/lib/systemd/system/psplash-network.service
/lib/systemd/system/psplash-basic.service
Please set FILES such that these items are packaged. Alternatively if they are unneeded, avoid installing them or delete them within do_install.
psplash: 2 installed and not shipped files. [installed-vs-shipped]
ERROR: psplash-0.1+gitAUTOINC+2015f7073e-r15 do_package: Fatal QA errors found, failing task.
ERROR: psplash-0.1+gitAUTOINC+2015f7073e-r15 do_package: Function failed: do_package
ERROR: Logfile of failure stored in: /home/zengguang/nxp_4.9.88/bld-agl/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/psplash/0.1+gitAUTOINC+2015f7073e-r15/temp/log.do_package.123587
ERROR: Task (/home/zengguang/nxp_4.9.88/sources/poky/meta/recipes-core/psplash/psplash_git.bb:do_package) failed with exit code '1'
Hi Guang Zeng,
I am facing the same error when building AGL Master sources. if you have resolved this please share your solution.
Hello Guang Zeng,
Are you following this guide?
https://source.codeaurora.org/external/imx/meta-nxp-agl/about/
If so, which version of Ubuntu are you using on your host? 16.04 is the recommended version as of today. I haven’t seen a similar error but I could try to reproduce it if you host is Ubuntu 16.04.
Regards,
hi gusarambula:
I used ubuntu16.04
I follow these step:
1、I modify local.conf,because my app needs qt5.9 support.
IMAGE_INSTALL_append = " qtbase qtbase-plugins qtwayland cinematicexperience liberation-fonts \
qtserialbus \
"
PACKAGECONFIG_FONTS_append_pn-qtbase = " fontconfig"
2、 $: bitbake agl-image-minimal
I download the image and ran the APP with an error after starting up.
error:
Failed to create display (No such file or directory)
3、$: bitbake agl-image-weston
compile error:
ERROR: psplash-0.1+gitAUTOINC+2015f7073e-r15 do_package: QA Issue: psplash: Files/directories were installed but not shipped in any package:
/lib/systemd/system/psplash-network.service
/lib/systemd/system/psplash-basic.service
4、$: bitbake agl-demo-platform
compile error,the error messeage is in the attachment
Hello Guang Zeng,
How did you solve this issue, iam also facing the same issue, pls reply with solution ... ???
ERROR: psplash-0.1+gitAUTOINC+2015f7073e-r15 do_package: QA Issue: psplash: Files/directories were installed but not shipped in any package:
/lib/systemd/system/psplash-basic.service
/lib/systemd/system/psplash-network.service
Please set FILES such that these items are packaged. Alternatively if they are unneeded, avoid installing them or delete them within do_install.
psplash: 2 installed and not shipped files. [installed-vs-shipped]
ERROR: psplash-0.1+gitAUTOINC+2015f7073e-r15 do_package: Fatal QA errors found, failing task.
ERROR: psplash-0.1+gitAUTOINC+2015f7073e-r15 do_package: Function failed: do_package
ERROR: Logfile of failure stored in: /home/imx8/weston-imx8/bld-agl/tmp/work/aarch64-poky-linux/psplash/0.1+gitAUTOINC+2015f7073e-r15/temp/log.do_package.23886
ERROR: Task (/home/imx8/weston-imx8/sources/poky/meta/recipes-core/psplash/psplash_git.bb:do_package) failed with exit code '1'
What is the solution to this issue ?
Regards
Mani