adv7533's driver for imx8qxp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

adv7533's driver for imx8qxp

1,204 Views
baijinlong
Contributor III

dear all:

      We have designed an adapter board with reference to IMX-MIPI-HDMI, but the IC is adv7533. We have modified the driver for the adv7535, but it does not work.
      Is there a driver for adv7533?

BSP:linux L4.14.98_2.0.0

Board: imx8qxp mek

0 Kudos
Reply
1 Reply

1,013 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jinlong 

there is adv7533 driver:

adv7533.c\adv7511\bridge\drm\gpu\drivers - linux-imx - i.MX Linux kernel 

one can put it along with adv7535 and debug, if necessary:

mxc\fbdev\video\drivers - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply