adding cups into LTIB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

adding cups into LTIB

2,116 次查看
LeeHong
Contributor I

Hi,

I am trying to add the package CUPS into LTIB.

However, I get this error when running scbuild.

I looked into the source file but nothing can be altered to redirect the /lib/ld-linux.so.3 which is in my target filesystem.

ERROR

Compressing cupsd.man... 56.0%
53.4%
51.6%
Converting man pages to HTML...
cancel.1.gz...
/lib/ld-linux.so.3: No such file or directory
cups-config.1.gz...
/lib/ld-linux.so.3: No such file or directory
cupstestdsc.1.gz...

Thanks.

标记 (1)
0 项奖励
回复
6 回复数

1,857 次查看
TomMorrison
Contributor III

Has anyone solved this problem - I REALLY would like to print captured / encoded images wireless to ad-hoc printer!

0 项奖励
回复

1,857 次查看
jimmychan
NXP TechSupport
NXP TechSupport

what is the BSP are you using?

0 项奖励
回复

1,857 次查看
TomMorrison
Contributor III

I am using the Freescale ER6-1209 release (that looks like came out last week).

I tried incorporating 1.3.11 (1.4.8 had MANY more issues than 1.3.11 did).

But, even then, there were multiple issues in the cross-compile (e.g.:do not create

the HTML output (because the compiled mantohtml doesn't run on host system)).

And, the final problem that I couldn't seem to get around was install script that

was having dependency issues for lib files (couldn't find them - due to NOT pointing

to the appropriate rootfs).

I gave up after that...for the moment.

got any suggestions?

tom

0 项奖励
回复

1,857 次查看
jimmychan
NXP TechSupport
NXP TechSupport

which board are you using?

0 项奖励
回复

1,857 次查看
TomMorrison
Contributor III

Boundary Devices Sabre Lite!

0 项奖励
回复

1,857 次查看
admin
Specialist II

pejmankalkhoran, can you help?

0 项奖励
回复