add file to boot partition of sdcard image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

add file to boot partition of sdcard image

1,836件の閲覧回数
rob_lepage
Contributor I

I am putting together an sdcard image to boot an imx.6ull and automatically program on board nand flash.  I am able to generate an sdcard image that boots and ubifs rootfs.  I have also increase the boot partition size in the sdcard image to make space for a copy of the ubifs.

My question is how can I have yocto automatically include the ubifs rootfs in the boot partition of the sdcard image?

Thanks for any help offered.

ラベル(2)
0 件の賞賛
返信
1 返信

1,696件の閲覧回数
b36401
NXP Employee
NXP Employee

You can refer to these yocto documents regarding to adding features:

https://community.nxp.com/docs/DOC-1616
https://community.nxp.com/docs/DOC-95333

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信