add OP-TEE with secure boot on IMX8MN

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

add OP-TEE with secure boot on IMX8MN

跳至解决方案
3,751 次查看
Silvarye
Contributor II

Hi all, 

I'm working on i.MX8M Nano board and I would like to know How can I add OP-TEE image in the secure boot.

With NXP's documentation I done this resume of commands (attached Notepad) ,  if I done something wrong say me, At which steps I could add commands for OP-TEE

Moreover, in your documentation for complete secure the device you purpose to do this : 

=> fuse prog 1 3 0x8000000 for Program DIR_BT_DIS

But in the security reference manual for IMX8MN, on 0x470[27] in Fuse map this appear like 'Reserved', It is important thing for the security ? 

Regards, 

Alexandre

0 项奖励
回复
1 解答
3,731 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Alexandre

 

from team:

 

1) In step 4, customer need to copy the tee.bin to the imx-mkimage tool. and compile the ATF with OP-TEE support. Then when customer build the image with the same command, the OP-TEE will integrated to the FIT part of the flash.bin. Customer can check the mkimage log to double confirm.

2) To close the device, customer need to use below command to program SEC_CONFIG[1] in bank1 word3, bit 25. 

  => fuse prog 1 3 0x2000000

 

Best regards
igor

在原帖中查看解决方案

3 回复数
3,727 次查看
Silvarye
Contributor II

Hi Igor thanks for your answer, have a nice day !

0 项奖励
回复
3,094 次查看
Murri
Contributor I

@Silvarye did this work for you? I am about to try the same. Thanks in advance. 

0 项奖励
回复
3,732 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Alexandre

 

from team:

 

1) In step 4, customer need to copy the tee.bin to the imx-mkimage tool. and compile the ATF with OP-TEE support. Then when customer build the image with the same command, the OP-TEE will integrated to the FIT part of the flash.bin. Customer can check the mkimage log to double confirm.

2) To close the device, customer need to use below command to program SEC_CONFIG[1] in bank1 word3, bit 25. 

  => fuse prog 1 3 0x2000000

 

Best regards
igor