my Image size bigger than 0x800000 so i change CONFIG_SYS_BOOTM_LEN
to increase "max gunzip size"
gedit /root/project_board/lollipop51/myandroid/bootable/bootloader/uboot-imx/common/bootm.c
//#define CONFIG_SYS_BOOTM_LEN 0x800000
//to
#define CONFIG_SYS_BOOTM_LEN 0x1000000
after build and reboot..............................................
Normal Boot
Hit any key to stop autoboot: 0
boota mmc1
kernel @ 14008000 (8817672)
ramdisk @ 15000000 (872002)
fdt @ 14f00000 (47600)
## Booting Android Image at 0x12000000 ...
Kernel load addr 0x14008000 size 8612 KiB
Kernel command line: console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:dev=hdmi,1920x1080M@60,if=RGB24,bpp=32 video=mxcfb2:off video=mxcfb3:off vmalloc=400M androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale cma=384M mem=1G firmware_class.path=/system/etc/firmware androidboot.selinux=disabled androidboot.dm_verity=disabled
## Flattened Device Tree blob at 14f00000
Booting using the fdt blob at 0x14f00000
Loading Kernel Image ... OK
Using Device Tree in place at 14f00000, end 14f0e9ef
switch to ldo_bypass mode!
Starting kernel ...
undefined instruction
pc : [<00010000>] lr : [<8fef2740>]
reloc pc : [<8791e000>] lr : [<17800740>]
sp : 8eeeda68 ip : 8eeeda44 fp : 00000000
r10: 00000000 r9 : 8eeedeb8 r8 : 009024b4
r7 : 000000f0 r6 : 00000098 r5 : 17800338 r4 : 00c5087d
r3 : 00000000 r2 : 00000000 r1 : 00000000 r0 : 00000000
Flags: NzCv IRQs off FIQs off Mode SVC_32
Resetting CPU ...
resetting ...
U-Boot 2015.04-svn62 (Mar 30 2016 - 18:03:51)
crash at static void v7_maint_dcache_all(u32 operation)
how to solve this problrm after add CONFIG_SYS_BOOTM_LEN size
Please note that if kernel exceeds 8M it may go beyond the boundaries of its place on SD card.
You need to modify card partition.
Please refer table in "Storage partitions" chapter of Android User's Guide.
And you need to change MFGtool configuration in point of the partitions.
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
do you mean mksdcard-android.sh.tar in mfg tools
# partition size in MB
BOOTLOAD_RESERVE=8
BOOT_ROM_SIZE=16
RECOVERY_ROM_SIZE=20
BOOTLOAD_RESERVE = 8 need bigger?
or the others
//#define CONFIG_SYS_BOOTM_LEN 0x800000
//to
#define CONFIG_SYS_BOOTM_LEN 0xA00000
also undefined instruction error
and my kernel size 8.6 mb
uboot makefile i use
ifdef CONFIG_CC_OPTIMIZE_FOR_SIZE
#KBUILD_CFLAGS += -Os
KBUILD_CFLAGS += -O0
else
KBUILD_CFLAGS += -O2
endif
when setting
KBUILD_CFLAGS += -O1 -fno-omit-frame-pointer
then run success
anyway other way setting
| KBUILD_CFLAGS | += -O0 |
and run success?
I got answer KBUILD_CFLAGS += -O0 and undefined instruction
/root/project_board/lollipop51/myandroid/bootable/bootloader/uboot-imx/Makefile
KBUILD_CFLAGS += -O0 -fno-omit-frame-pointer
/root/project_board/lollipop51/myandroid/bootable/bootloader/uboot-imx/arch/arm/lib/cache-cp15.c
static void cache_disable(uint32_t cache_bit)
if (cache_bit == (CR_C | CR_M))
{
flush_dcache_all();
/* issue begin */
/*
set_cr(reg & ~CR_C);
flush_dcache_all(); //overwrite memory here
*/
}
find problem
set_cr(reg & ~CR_C); //disable data cache
flush_dcache_all(); //will way/set data cacahe
there will be problem on i.mx6
this is add on i.mx7
remove them is ok~~~ on i.mx6 and i.mx7
you can use -O0 build and test code will find this problem