adb over network through sdcard booting (Android)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

adb over network through sdcard booting (Android)

827 次查看
chandrasekharma
Contributor III

Hi all,

I enabled one property service.adb.tcp.port 5555 for adb over network. Its working fine after typing command

adb connect <ip-address> in emmc booting for android 5.0.2 and its not working after typing command

adb connect <ip-address> in sdcard booting for android 5.0.2 with same device but difference is only booting mode. Please help me any extra property i need to add for adb over network through sdcard booting.

Thanks in advance

标签 (3)
0 项奖励
回复
1 回复

758 次查看
b36401
NXP Employee
NXP Employee

Please make sure that the network is configured correctly in SD-card case.

I mean please try to perform some other TCP connection between the board and host machine.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复