adb devices

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

adb devices

8,528 Views
mehulshah
Contributor III

Hi ,

I  am able to get prompt on the devices ; but when i do "adb devices" on host side , i am not seeing any device..can you please let me know , what is missing. here the log(no option for attachment)

U-Boot 2015.04-14490-g596b7a8-dirty (Mar 07 2017 - 19:43:47)

CPU:   Freescale i.MX7D rev1.2 at 792 MHz
CPU:   Temperature 33 C
Reset cause: POR
Board: i.MX7D SABRESD RevA
I2C:   ready
DRAM:  1 GiB
PMIC: PFUZE300 DEV_ID=0x30 REV_ID=0x11
MMC:   FSL_SDHC: 0, FSL_SDHC: 1
*** Warning - bad CRC, using default environment

No panel detected: default to TFT43AB
Display: TFT43AB (480x272)
Video: 480x272x24
In:    serial
Out:   serial
Err:   serial
check_and_clean: reg 0, flag_set 0
Fastboot: Normal
flash target is MMC:0
Net:   FEC0
Normal Boot
Hit any key to stop autoboot:  3     2     1     0
boota mmc0
kernel   @ 82808000 (8722272)
ramdisk  @ 83800000 (1071037)
fdt      @ 83700000 (48214)
## Booting Android Image at 0x80800000 ...
Kernel load addr 0x82808000 size 8518 KiB
Kernel command line: console=ttymxc0,115200 init=/init androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale
## Flattened Device Tree blob at 83700000
   Booting using the fdt blob at 0x83700000
   Loading Kernel Image ... OK
   Using Device Tree in place at 83700000, end 8370ec55

Starting kernel ...

Booting Linux on physical CPU 0x0
Initializing cgroup subsys cpu
Initializing cgroup subsys cpuacct
Linux version 4.1.15 (root@ubuntu) (gcc version 4.9.x-google 20140827 (prerelease) (GCC) ) #5 SMP PREEMPT Fri Mar 3 20:40:47 IST 2017
CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine model: Freescale i.MX7D SabreSD Board
Reserved memory: created CMA memory pool at 0x9a000000, size 320 MiB
Reserved memory: initialized node linux,cma, compatible id shared-dma-pool
Memory policy: Data cache writealloc
PERCPU: Embedded 13 pages/cpu @eef18000 s22144 r8192 d22912 u53248
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 260368
Kernel command line: console=ttymxc0,115200 init=/init androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale androidboot.serialno=0000023674a400d3
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 690844K/1047552K available (11566K kernel code, 978K rwdata, 3688K rodata, 1024K init, 653K bss, 29028K reserved, 327680K cma-reserved, 269312K highmem)
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
    vmalloc : 0xf0000000 - 0xff000000   ( 240 MB)
    lowmem  : 0xc0000000 - 0xef800000   ( 760 MB)
    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
    modules : 0xbf000000 - 0xbfe00000   (  14 MB)
      .text : 0xc0008000 - 0xc0fe59fc   (16247 kB)
      .init : 0xc1000000 - 0xc1100000   (1024 kB)
      .data : 0xc1100000 - 0xc11f4890   ( 979 kB)
       .bss : 0xc11f4890 - 0xc1297f64   ( 654 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
Preemptible hierarchical RCU implementation.
    Additional per-CPU info printed with stalls.
    RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
NR_IRQS:16 nr_irqs:16 16
Architected cp15 timer(s) running at 8.00MHz (phys).
clocksource arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns
sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns
Switching to timer-based delay loop, resolution 125ns
mxc_clocksource_init 3000000
Ignoring duplicate/late registration of read_current_timer delay
clocksource mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=80000)
pid_max: default: 32768 minimum: 301
Security Framework initialized
SELinux:  Initializing.
AppArmor: AppArmor disabled by boot time parameter
Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
Initializing cgroup subsys freezer
Initializing cgroup subsys debug
CPU: Testing write buffer coherency: ok
/cpus/cpu@0 missing clock-frequency property
/cpus/cpu@1 missing clock-frequency property
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x80100000 - 0x80100058
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
Brought up 2 CPUs
SMP: Total of 2 processors activated (32.00 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
device-tree: Duplicate name in lcdif@30730000, renamed to "display#1"
VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5
clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor ladder
cpuidle: using governor menu
DDR type is DDR3!
hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 8 bytes.
VDSO is not a valid ELF object!
imx7d-pinctrl 302c0000.iomuxc-lpsr: initialized IMX pinctrl driver
imx7d-pinctrl 30330000.iomuxc: initialized IMX pinctrl driver
MU is ready for cross core communication!
mxs-dma 33000000.dma-apbh: initialized
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
30800000.aips-bus:usbphy_nop1 supply vcc not found, using dummy regulator
30800000.aips-bus:usbphy_nop2 supply vcc not found, using dummy regulator
i2c i2c-0: IMX I2C adapter registered
i2c i2c-0: can't use DMA
i2c i2c-1: IMX I2C adapter registered
i2c i2c-1: can't use DMA
i2c i2c-2: IMX I2C adapter registered
i2c i2c-2: can't use DMA
i2c i2c-3: IMX I2C adapter registered
i2c i2c-3: can't use DMA
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Initialized.
Bluetooth: Core ver 2.20
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
Switched to clocksource arch_sys_counter
NET: Registered protocol family 2
TCP established hash table entries: 8192 (order: 3, 32768 bytes)
TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
Freeing initrd memory: 1048K (c3800000 - c3906000)
imx rpmsg driver is registered.
Bus freq driver module loaded
console [pstore-1] enabled
pstore: Registered ramoops as persistent store backend
ramoops: attached 0x100000@0xbbf00000, ecc: 0/0
mxc_ramoops device success loaded
bt power gpio is:119
rfkill: BT RF going to : on
mxc_bt_rfkill_reset
mxc_bt_rfkill driver success loaded
futex hash table entries: 512 (order: 3, 32768 bytes)
audit: initializing netlink subsys (disabled)
audit: type=2000 audit(0.430:1): initialized
VFS: Disk quotas dquot_6.6.0
VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
ntfs: driver 2.1.32 [Flags: R/W DEBUG].
jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
fuse init (API version 7.23)
bounce: pool size: 64 pages
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
pwm-backlight supply power not found, using dummy regulator
MIPI DSI driver module loaded
MIPI DSI driver module loaded
sii902x 2-0039: No reset pin found
sii902x 2-0039: Can not read edid
30730000.lcdif supply lcd not found, using dummy regulator
mxsfb 30730000.lcdif: failed to find mxc display driver
Console: switching to colour frame buffer device 60x34
mxsfb 30730000.lcdif: initialized
imx-sdma 30bd0000.sdma: no event needs to be remapped
imx-sdma 30bd0000.sdma: loaded firmware 4.2
imx-sdma 30bd0000.sdma: initialized
pfuze100-regulator 0-0008: Full layer: 1, Metal layer: 1
pfuze100-regulator 0-0008: FAB: 0, FIN: 0
pfuze100-regulator 0-0008: pfuze3000 found.
30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 279, base_baud = 1500000) is a IMX
console [ttymxc0] enabled
30a70000.serial: ttymxc4 at MMIO 0x30a70000 (irq = 288, base_baud = 5000000) is a IMX
30a80000.serial: ttymxc5 at MMIO 0x30a80000 (irq = 289, base_baud = 5000000) is a IMX
imx sema4 driver is registered.
[drm] Initialized drm 1.1.0 20060810
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
zram: Created 1 device(s)
input: fxos8700 as /devices/platform/soc/30800000.aips-bus/30a30000.i2c/i2c-1/1-001e/input/input0
fxos8700 device driver probe successfully
input: fxas2100x as /devices/platform/soc/30800000.aips-bus/30a30000.i2c/i2c-1/1-0020/input/input1
fxas2100x 1-0020: fxas2100x device driver probe successfully
spi_gpio spi4: gpio-miso property not found, switching to no-rx mode
spi_imx 30840000.ecspi: probed
tun: Universal TUN/TAP device driver, 1.6
tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
CAN device driver interface
flexcan 30a10000.can: device registered (reg_base=f5a10000, irq=283)
30be0000.ethernet supply phy not found, using dummy regulator
pps pps0: new PPS source ptp0
libphy: fec_enet_mii_bus: probed
fec 30be0000.ethernet eth0: registered PHC device 0
30bf0000.ethernet supply phy not found, using dummy regulator
pps pps1: new PPS source ptp1
fec 30bf0000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00
fec 30bf0000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: b6:d4:d1:fb:43:8e
fec 30bf0000.ethernet eth1: registered PHC device 1
PPP generic driver version 2.4.2
PPP BSD Compression module registered
PPP Deflate Compression module registered
PPP MPPE Compression module registered
NET: Registered protocol family 24
pegasus: v0.9.3 (2013/04/25), Pegasus/Pegasus II USB Ethernet driver
usbcore: registered new interface driver pegasus
usbcore: registered new interface driver rtl8150
usbcore: registered new interface driver r8152
usbcore: registered new interface driver asix
usbcore: registered new interface driver ax88179_178a
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver cdc_eem
usbcore: registered new interface driver net1080
usbcore: registered new interface driver cdc_subset
usbcore: registered new interface driver zaurus
usbcore: registered new interface driver cdc_ncm
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver cdc_acm
cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
usbcore: registered new interface driver usb-storage
usbcore: registered new interface driver usbserial
usbcore: registered new interface driver usbserial_generic
usbserial: USB Serial support registered for generic
usbcore: registered new interface driver ftdi_sio
usbserial: USB Serial support registered for FTDI USB Serial Device
usbcore: registered new interface driver option
usbserial: USB Serial support registered for GSM modem (1-port)
usbcore: registered new interface driver usb_ehset_test
30b10200.usbmisc supply vbus-wakeup not found, using dummy regulator
30b20200.usbmisc supply vbus-wakeup not found, using dummy regulator
30b30200.usbmisc supply vbus-wakeup not found, using dummy regulator
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: EHCI Host Controller
usb usb1: Manufacturer: Linux 4.1.15 ehci_hcd
usb usb1: SerialNumber: ci_hdrc.1
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mousedev: PS/2 mouse device common for all mice
input: 30370000.snvs:snvs-powerkey as /devices/platform/soc/30000000.aips-bus/30370000.snvs/30370000.snvs:snvs-powerkey/input/input2
usbcore: registered new interface driver xpad
usbcore: registered new interface driver usb_acecad
usbcore: registered new interface driver aiptek
usbcore: registered new interface driver gtco
usbcore: registered new interface driver hanwang
usbcore: registered new interface driver kbtab
spi2.0 supply vcc not found, using dummy regulator
ads7846 spi2.0: touchscreen, irq 88
input: ADS7846 Touchscreen as /devices/platform/soc/30800000.aips-bus/30800000.spba-bus/30840000.ecspi/spi_master/spi2/spi2.0/input/input3
read mpl3115 chip id 0xc4
input: mpl3115 as /devices/virtual/input/input4
mpl3115 device driver probe successfully
snvs_rtc 30370000.snvs:snvs-rtc-lp: rtc core: registered 30370000.snvs:snvs- as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x/sz) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR SANYO protocol handler initialized
IR Sharp protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
IR XMP protocol handler initialized
mxc_mipi-csi 30750000.mipi-csi: mipi csi v4l2 device registered
CSI: Registered sensor subdevice: mxc_mipi-csi.0
mxc_mipi-csi 30750000.mipi-csi: lanes: 2, hs_settle: 13, wclk: 1, freq: 240000000
ov5647_mipi 3-0036: no  pin available
ov5647_mipi 3-0036: no sensor reset pin available
3-0036 supply DOVDD not found, using dummy regulator
3-0036 supply DVDD not found, using dummy regulator
3-0036 supply AVDD not found, using dummy regulator
ov5647_read_reg:write reg error:reg=300a
camera ov5647_mipi is not found
pxp-v4l2 pxp_v4l2_out: initialized
usbcore: registered new interface driver uvcvideo
USB Video Class driver (1.1.1)
imx2-wdt 30280000.wdog: use WDOG_B to reboot.
imx2-wdt 30280000.wdog: timeout 60 sec (nowayout=0)
device-mapper: uevent: version 1.0.3
device-mapper: ioctl: 4.31.0-ioctl (2015-3-12) initialised: dm-devel@redhat.com
Bluetooth: HCI UART driver ver 2.3
Bluetooth: HCI UART protocol H4 registered
Bluetooth: HCI UART protocol BCSP registered
Bluetooth: HCI UART protocol ATH3K registered
usbcore: registered new interface driver btusb
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
/soc/aips-bus@30800000/usdhc@30b40000: voltage-ranges unspecified
sdhci-esdhc-imx 30b40000.usdhc: Got CD GPIO
sdhci-esdhc-imx 30b40000.usdhc: Got WP GPIO
sdhci-esdhc-imx 30b40000.usdhc: No vqmmc regulator found
mmc0: SDHCI controller on 30b40000.usdhc [30b40000.usdhc] using ADMA
/soc/aips-bus@30800000/usdhc@30b50000: voltage-ranges unspecified
sdhci-esdhc-imx 30b50000.usdhc: assigned as wifi host
sdhci-esdhc-imx 30b50000.usdhc: No vmmc regulator found
sdhci-esdhc-imx 30b50000.usdhc: No vqmmc regulator found
mmc1: SDHCI controller on 30b50000.usdhc [30b50000.usdhc] using ADMA
/soc/aips-bus@30800000/usdhc@30b60000: voltage-ranges unspecified
sdhci-esdhc-imx 30b60000.usdhc: No vmmc regulator found
sdhci-esdhc-imx 30b60000.usdhc: No vqmmc regulator found
mmc2: SDHCI controller on 30b60000.usdhc [30b60000.usdhc] using ADMA
caam 30900000.caam: Entropy delay = 3200
caam 30900000.caam: Instantiated RNG4 SH0
caam 30900000.caam: Instantiated RNG4 SH1
caam 30900000.caam: device ID = 0x0a16030000000000 (Era -524)
caam 30900000.caam: job rings = 3, qi = 0
mmc0: new ultra high speed SDR104 SDHC card at address 0007
mmcblk0: mmc0:0007 SL16G 14.4 GiB
 mmcblk0: p1 p2 p3 < p5 p6 p7 p8 p9 > p4
caam algorithms registered in /proc/crypto
caam_jr 30901000.jr0: registering rng-caam
platform caam_sm: blkkey_ex: 8 keystore units available
platform caam_sm: 64-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: 64-bit black key:
platform caam_sm: [0000] 95 7c 6a f5 66 70 89 b3
platform caam_sm: [0008] c5 76 50 2b e6 dd 3d 2f
platform caam_sm: 128-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: 128-bit black key:
platform caam_sm: [0000] 7b 3c dc dc 09 1d fb 2d
platform caam_sm: [0008] 91 c6 0e 2c 9a 89 8e c2
platform caam_sm: 192-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: [0016] 10 11 12 13 14 15 16 17
platform caam_sm: 192-bit black key:
platform caam_sm: [0000] aa b2 91 1b 36 11 ea b4
platform caam_sm: [0008] 92 5a 43 16 1a cf ed b4
platform caam_sm: [0016] 9b 86 4c f3 1f c4 52 ce
platform caam_sm: [0024] 5d f7 1d af e5 89 c7 d3
platform caam_sm: 256-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: [0016] 10 11 12 13 14 15 16 17
platform caam_sm: [0024] 18 19 1a 1b 1c 1d 1e 1f
platform caam_sm: 256-bit black key:
platform caam_sm: [0000] 70 88 5d 00 73 04 a9 92
platform caam_sm: [0008] 6c 7a 73 f9 bd 9e df 28
platform caam_sm: [0016] 51 55 6b 70 4a 50 33 b8
platform caam_sm: [0024] 97 95 79 c0 90 c4 29 b2
platform caam_sm: 64-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 128-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 196-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 256-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 64-bit black key in blob:
platform caam_sm: [0000] a8 52 88 70 bb f2 c1 2c
platform caam_sm: [0008] 4f 63 88 0b b3 9f 9e fc
platform caam_sm: [0016] 41 a6 cb 3c b9 91 1d 4a
platform caam_sm: [0024] 10 13 7e 9f 47 ee 68 bf
platform caam_sm: [0032] 35 59 fd 7c 0e a5 00 ab
platform caam_sm: [0040] b7 e9 80 eb 36 cd 73 a3
platform caam_sm: [0048] ce d2 80 9e 88 99 79 06
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 128-bit black key in blob:
platform caam_sm: [0000] 14 bf 9b 16 da 79 41 3f
platform caam_sm: [0008] 14 6f 2e 1c 2e 1a 58 3d
platform caam_sm: [0016] 0e 9d 7b 55 e1 6e 53 e4
platform caam_sm: [0024] 17 8e 5c 58 3c 05 4c f1
platform caam_sm: [0032] 55 d9 ef 4b ba ed 5d 03
platform caam_sm: [0040] c0 cf 77 e9 d8 38 01 05
platform caam_sm: [0048] 5f 84 bf d2 19 ba 37 e9
platform caam_sm: [0056] b8 17 7a 14 78 4a 97 53
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 192-bit black key in blob:
platform caam_sm: [0000] d0 cf 2d 21 b8 a2 89 9d
platform caam_sm: [0008] 3d 73 e8 1f ec 8e 16 94
platform caam_sm: [0016] ad 76 63 3b a0 a0 b3 f0
platform caam_sm: [0024] f6 42 d6 dc fc 81 83 1d
platform caam_sm: [0032] ca 56 8c a6 2e e3 12 6b
platform caam_sm: [0040] 76 0a 8b b5 8c c6 e8 ab
platform caam_sm: [0048] e1 64 30 28 9a 75 72 a9
platform caam_sm: [0056] 59 bf e5 2d 4f 52 5a 69
platform caam_sm: [0064] d6 55 9a 54 df 37 5b df
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 256-bit black key in blob:
platform caam_sm: [0000] f3 ea a7 1c 67 3d 8a 43
platform caam_sm: [0008] 87 ef 08 72 08 ba ab 46
platform caam_sm: [0016] 41 b8 79 eb 2c 13 0b 1b
platform caam_sm: [0024] 89 bd d5 81 eb 3f 52 0d
platform caam_sm: [0032] 19 65 fe 9b 90 16 d6 36
platform caam_sm: [0040] f4 40 ce 1e c2 7a 20 07
platform caam_sm: [0048] 92 ac 67 e5 e7 b3 03 ff
platform caam_sm: [0056] ef 25 28 d3 32 31 a6 27
platform caam_sm: [0064] 29 8e 0f c9 f4 1a f2 7f
platform caam_sm: [0072] f6 c1 60 de c5 d0 8e 4a
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: restored 64-bit black key:
platform caam_sm: [0000] cb 3c 2e e2 31 25 db 16
platform caam_sm: [0008] 5d 8c 17 1d db 6d be 3b
platform caam_sm: restored 128-bit black key:
platform caam_sm: [0000] 7b 3c dc dc 09 1d fb 2d
platform caam_sm: [0008] 91 c6 0e 2c 9a 89 8e c2
platform caam_sm: restored 192-bit black key:
platform caam_sm: [0000] aa b2 91 1b 36 11 ea b4
platform caam_sm: [0008] 92 5a 43 16 1a cf ed b4
platform caam_sm: [0016] dc a4 c9 63 e5 4f 0b 02
platform caam_sm: [0024] 26 af 0e 1b 70 6d 1f 90
platform caam_sm: restored 256-bit black key:
platform caam_sm: [0000] 70 88 5d 00 73 04 a9 92
platform caam_sm: [0008] 6c 7a 73 f9 bd 9e df 28
platform caam_sm: [0016] 51 55 6b 70 4a 50 33 b8
platform caam_sm: [0024] 97 95 79 c0 90 c4 29 b2
snvs-secvio 30370000.caam-snvs: can't get snvs clock
snvs-secvio 30370000.caam-snvs: violation handlers armed - non-secure state
hidraw: raw HID events driver (C) Jiri Kosina
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
ashmem: initialized
usbcore: registered new interface driver snd-usb-audio
imx-wm8960 sound: wm8960-hifi <-> 308a0000.sai mapping ok
imx-sii902x sound-hdmi: snd-soc-dummy-dai <-> 308c0000.sai mapping ok
NET: Registered protocol family 26
u32 classifier
    Actions configured
Netfilter messages via NETLINK v0.30.
nf_conntrack version 0.5.0 (15930 buckets, 63720 max)
ctnetlink v0.93: registering with nfnetlink.
xt_time: kernel timezone is -0000
ip_tables: (C) 2000-2006 Netfilter Core Team
arp_tables: (C) 2002 David S. Miller
Initializing XFRM netlink socket
NET: Registered protocol family 10
mip6: Mobile IPv6
ip6_tables: (C) 2000-2006 Netfilter Core Team
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
NET: Registered protocol family 15
can: controller area network core (rev 20120528 abi 9)
NET: Registered protocol family 29
can: raw protocol (rev 20120528)
can: broadcast manager protocol (rev 20120528 t)
can: netlink gateway (rev 20130117) max_hops=1
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: BNEP socket layer initialized
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
Bluetooth: HIDP socket layer initialized
8021q: 802.1Q VLAN Support v1.8
Key type dns_resolver registered
cpu cpu0: dev_pm_opp_get_opp_count: device OPP not found (-19)
dhd_module_init in
Power-up adapter 'DHD generic adapter'
wifi_platform_bus_enumerate device present 1
mmc1: queuing unknown CIS tuple 0x80 (2 bytes)
mmc1: queuing unknown CIS tuple 0x80 (7 bytes)
mmc1: queuing unknown CIS tuple 0x80 (6 bytes)
mmc1: queuing unknown CIS tuple 0x91 (3 bytes)
mmc1: new ultra high speed SDR104 SDIO card at address 0001
F1 signature OK, socitype:0x1 chip:0x4339 rev:0x1 pkg:0x0
DHD: dongle ram size is set to 786432(orig 786432) at 0x180000
wifi_platform_get_mac_addr
CFG80211-ERROR) wl_setup_wiphy : Registering Vendor80211)
wl_create_event_handler(): thread:wl_event_handler:a0 started
CFG80211-ERROR) wl_event_handler :
dhd_attach(): thread:dhd_watchdog_thread:a1 started
tsk Enter, tsk = 0xd892147c
dhd_attach(): thread:dhd_dpc:a2 started
dhd_deferred_work_init: work queue initialized

Dongle Host Driver, version 1.141.88 (r)
Compiled from
Register interface [wlan0]  MAC: 00:90:4c:11:22:33

CFG80211-ERROR) wl_event_handler : was terminated
wl_destroy_event_handler(): thread:wl_event_handler:a0 terminated OK
dhd_prot_ioctl : bus is down. we have nothing to do
input: gpio-keys as /devices/platform/gpio-keys/input/input6
snvs_rtc 30370000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:00:02 UTC (2)
wlreg_on: disabling
vref-1v8: disabling
can2-3v3: disabling
usb_otg1_vbus: disabling
ALSA device list:
  #0: wm8960-audio
  #1: sii902x-audio
Freeing unused kernel memory: 1024K (c1000000 - c1100000)
init: init started!
SELinux:  Android master kernel running Android M policy in compatibility mode.
SELinux:  Permission audit_read in class capability2 not defined in policy.
SELinux: the above unknown classes and permissions will be denied
audit: type=1403 audit(2.660:2): policy loaded auid=4294967295 ses=4294967295
audit: type=1404 audit(2.680:3): enforcing=1 old_enforcing=0 auid=4294967295 ses=4294967295
init: (Initializing SELinux enforcing took 0.13s.)
init: init second stage started!
init: waitpid failed: No child processes
init: property_set("ro.zygote", "zygote32") failed
init: (Loading properties from /default.prop took 0.00s.)
init: (Parsing /init.environ.rc took 0.00s.)
init: (Parsing /init.usb.rc took 0.00s.)
init: (Parsing init.freescale.usb.rc took 0.00s.)
init: (Parsing /init.freescale.rc took 0.01s.)
init: (Parsing /init.usb.configfs.rc took 0.00s.)
init: (Parsing /init.zygote32.rc took 0.00s.)
init: (Parsing /init.trace.rc took 0.00s.)
init: (Parsing /init.rc took 0.03s.)
init: SELinux: Could not get canonical path /adb_keys restorecon: No such file or directory.
init: Starting service 'ueventd'...
audit: type=1400 audit(2.830:4): avc:  denied  { mounton } for  pid=1 comm="init" path="/sys/kernel/debug" dev="debugfs" ino=1 scontext=u:r:init:s0 tcontext=u:object_r:debugfs:s0 tclass=dir permissive=0
ueventd: ueventd started!
init: Waiting for /dev/.coldboot_done...
ueventd: Coldboot took 0.30s.
init: Waiting for /dev/.coldboot_done took 0.30s.
init: write_file: Unable to open '/proc/sys/kernel/sched_compat_yield': No such file or directory
init: write_file: Unable to write to '/dev/cpuctl/cpu.shares': Invalid argument
init: write_file: Unable to open '/proc/sys/abi/swp': No such file or directory
Console: switching to colour dummy device 80x30
EXT4-fs (mmcblk0p5): mounted filesystem with ordered data mode. Opts: barrier=1
fs_mgr: __mount(source=/dev/block/mmcblk0p5,target=/system,type=ext4)=0
EXT4-fs (mmcblk0p4): Ignoring removed nomblk_io_submit option
EXT4-fs (mmcblk0p4): recovery complete
EXT4-fs (mmcblk0p4): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic
fs_mgr: __mount(source=/dev/block/mmcblk0p4,target=/data,type=ext4)=0
EXT4-fs (mmcblk0p6): Ignoring removed nomblk_io_submit option
EXT4-fs (mmcblk0p6): recovery complete
EXT4-fs (mmcblk0p6): mounted filesystem with ordered data mode. Opts: nomblk_io_submit
fs_mgr: __mount(source=/dev/block/mmcblk0p6,target=/cache,type=ext4)=0
EXT4-fs (mmcblk0p7): mounted filesystem with ordered data mode. Opts: (null)
fs_mgr: __mount(source=/dev/block/mmcblk0p7,target=/device,type=ext4)=0
file system registered
init: Starting service 'logd'...
zram0: detected capacity change from 0 to 314572800
audit: type=1400 audit(15.370:5): avc:  denied  { read write } for  pid=179 comm="mkswap" name="zram0" dev="tmpfs" ino=7380 scontext=u:r:toolbox:s0 tcontext=u:object_r:block_device:s0 tclass=blk_file permissive=0
logd.auditd: start
logd.klogd: 18260750625
Unable to find swap-space signature
fs_mgr: swapon failed for /dev/block/zram0
init: (Loading properties from /system/build.prop took 0.01s.)
init: (Loading properties from /vendor/build.prop took 0.00s.)
init: (Loading properties from /factory/factory.prop took 0.00s.)
init: Starting service 'vold'...
init: Not bootcharting.
init: Starting service 'exec 0 (/system/bin/tzdatacheck)'...
init: Service 'exec 0 (/system/bin/tzdatacheck)' (pid 188) exited with status 0
init: (Loading properties from /data/local.prop took 0.00s.)
random: init urandom read with 35 bits of entropy available
init: Starting service 'logd-reinit'...
init: Starting service 'healthd'...
init: Starting service 'console'...
init: Starting service 'lmkd'...
init: Starting service 'servicemanager'...
binder: 190:190 transaction failed 29189, size 0-0
init: Starting service 'surÿinit: write_file: Unable to open '/sys/block/mmcblk1/queue/read_ahead_kb': No such file or directory
rfkill: BT RF going to : off
logd.daemon: reinit
type=1400 audit(17.300:6): avc: denied { dac_override } for pid=191 comm="sh" capability=1 scontext=u:r:shell:s0 tcontext=u:r:shell:s0 tclass=capability permissive=0
root@sabresd_7d:/ # healthd: No charger supplies found
healthd: No battery devices found
init: Service 'logd-reinit' (pid 189) exited with status 0
type=1400 audit(22.790:7): avc: denied { write } for pid=1 comm="init" name="galcore" dev="sysfs" ino=13324 scontext=u:r:init:s0 tcontext=u:object_r:sysfs:s0 tclass=dir permissive=0
init: write_file: Unable to open '/sys/bus/platform/drivers/galcore/gpu3DMinClock': Permission denied
init: property_set("ro.ril.wake_lock_timeout", "300") failed
init: Starting service 'netd'...
init: Starting service 'debuggerd'...
init: cannot find '/system/bin/debuggerd64', disabling 'debuggerd64'
init: Starting service 'drm'...
init: Starting service 'media'...
init: Starting service 'installd'...
init: cannot find '/system/bin/install-recovery.sh', disabling 'flash_recovery'
init: Starting service 'keystore'...
init: Starting service 'ril-daemon'...
init: Starting service 'zygote'...
init: Starting service 'gatekeeperd'...
init: Starting service 'perfprofd'...
init: Starting service 'sensor_fusion'...
init: Starting service 'adbd'...
read descriptors
read strings
input: FSL_SENS_HUB as /devices/virtual/input/input7
init: Starting service 'bootanim'...

root@sabresd_7d:/ # random: nonblocking pool is initialized

root@sabresd_7d:/ #

0 Kudos
Reply
10 Replies

6,619 Views
chum
Contributor III

I'm also getting same log.

adb device command didn't find imx6q board on host machine

i'm using sdcard with android oreo image

0 Kudos
Reply

6,619 Views
xinyu_chen
NXP Employee
NXP Employee

Windows PC or Linux PC? Have you enabled the ADB in the Settings?

0 Kudos
Reply

6,619 Views
mehulshah
Contributor III

Hi Eric,

I  am using Ubuntu-16.04 Linux machine..please reply....how to enable ADB in settings ?

Thanks ,

Mehul

0 Kudos
Reply

6,619 Views
xinyu_chen
NXP Employee
NXP Employee
0 Kudos
Reply

6,619 Views
mehulshah
Contributor III

Hi Eric ,

I want steps for linux(Ubuntu) . in the link you given is for windows .

Regards,

Mehul

0 Kudos
Reply

6,619 Views
xinyu_chen
NXP Employee
NXP Employee

They're same

0 Kudos
Reply

6,619 Views
mehulshah
Contributor III

in the android code  ? where i have to enable the settings ???

0 Kudos
Reply

6,619 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Mehul Shah,

You need to enable USB debugging in order to enable ADB. You can see instructions on how to do this on the following document. It is based on an older Android release but the procedure is basically the same.

https://community.nxp.com/docs/DOC-102514 

I hope this helps!

Regards,

0 Kudos
Reply

6,619 Views
mehulshah
Contributor III

Hi Gusarambula,

Thanks for reply..

I am using the Ubuntu 16.04 as host machine...please send the link for setting up ADB devices on ubuntu machine.

Regards,

Mehul

0 Kudos
Reply

6,619 Views
mehulshah
Contributor III

Ubuntu system....i have installed ADB in the host system.

0 Kudos
Reply