activate ENET in MCUXpresso

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

activate ENET in MCUXpresso

2,454件の閲覧回数
ingdb
Contributor III

Hello all,

I am using "MCUXpresso IDE v11.5.0 [Build 7232]", after setting up an MCU project for RT1173 or 75 or 76, the ENET either as 10/100 or G Ethernet does not show up in the peripheral list. Any suggestion or help on how to activate and add ENET to the project?

 

Best regards

Matthias

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,420件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Are you talking about this kind of screenshot?
-- Yes, and after confirming, so far, the MCUXpresso Config Tools hasn't integrated the ENET module in the peripheral item.
Hope this is clear.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,442件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi @ingdb ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I was wondering if you can share some screenshots to present your question.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,429件の閲覧回数
ingdb
Contributor III

Hi TIC,

are you talking about this kind of screenshot?

 

best regards

Matthias

0 件の賞賛
返信