absolute maximum ratings for HDMI signals and clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

absolute maximum ratings for HDMI signals and clock

674 Views
diegoperez
Contributor II

Hi,

What is the absolute maximum ratings for HDMI signals and clock? in the imx6 processor:

HDMI_CLKM

HDMI_CLKP

HDMI_D0M
HDMI_D0P

HDMI_D1M

HDMI_D1P

HDMI_D2M
HDMI_D2P

BR

Diego.

Labels (6)
0 Kudos
2 Replies

569 Views
diegoperez
Contributor II

Hi Igor,

I see in table 59 that the termination voltage of the receiver must be between 3.15 and 3.45. These are the operating conditions, but I would like to know the maximum ratings.

I am studying a problem that causes imx hdmi phy to break, and I suspect it could be due to a transient voltage at power up of receiver board.

BR 

Diego.

0 Kudos

569 Views
igorpadykov
NXP Employee
NXP Employee

Hi Diego

it can be found in sect.4.12.7.2 Electrical Characteristics

i.MX 6Dual/6Quad Applications Processors for Consumer Products - Data Sheet

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos