about x11 display on imx6sl EPD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about x11 display on imx6sl EPD

881 Views
guoxiongjiang
Contributor II

Hi,

I am testing X11 display on EPD of nxp imx6sl_evk. i build the software using fsl-yocto-L4.1.15_2.0.0-ga package.

DISTRO=fsl-imx-x11 MACHINE=imx6slevk source fsl-setup-release.sh -b build-x11-imx6sl

bitbake fsl-image-gui

Now I boot the imx6sl_evk and run /unit_test/mxc_epdc_fb.out, the EPD works well, but how can I get "mxc_epdc_x11_fb_test.out" ?  in the "unit_test" directory, I only can find  the two files: mxc_epdc_fb.out and mxc_epdc_v2_fb.out.

 Regards,

Jiang

Labels (1)
0 Kudos
Reply
1 Reply

805 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jiang

there are no special x11 unit tests, in unit_test one can find test sources

which can be used for custom testing or developing new drivers.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------.

0 Kudos
Reply