about uuu document

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about uuu document

1,837 Views
HEXER
Contributor III

Greetings community.

Am i the only one who thinks UUU pdf file's content has lots of grammatically incorrect sentences?

I don't want to be ungraceful. I am asking because i am also a non-native English speaker and i want to see correct sentences to improve/educate myself.

 

Best regards...

Tags (1)
0 Kudos
Reply
5 Replies

1,802 Views
HEXER
Contributor III

I was referring to https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/imx-processors/140261/1/UUU.pdf

for example:

UUU design as common library and UI. So user can easily integrate into their tools with uuu library. UUU also easy run in any
scripts.

and

bootloader means bootable image, which included ROM required header. for imx6/7, it should be uboot.imx
generally. for imx8qxp\imx8qm\imx8mm\im8mq, it is flash.bin.

i find the sentences quite weird.

0 Kudos
Reply

1,772 Views
Mestkim
Contributor III

兄弟这个不是汉语拼音

0 Kudos
Reply

1,784 Views
Mestkim
Contributor III

I read the words, it is very clear. 

And I also put the words into to word to check. Here is result. It seems no grammar issue there.

 

2023-08-04_110603.png

 

 

 

 

 

0 Kudos
Reply

1,744 Views
HEXER
Contributor III

It seems that the issue is my bad english.

0 Kudos
Reply

1,821 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @HEXER !

Could you please point to me what uuu.pdf are you referring?

And if you can point which sentences are incorrect.

 

Best regards.

0 Kudos
Reply