about the camera interface for ov8820

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

about the camera interface for ov8820

ソリューションへジャンプ
2,063件の閲覧回数
erichu
Contributor II

I am working on the camera interface of ov8820 for sabresd board. i suppose these are out of box function modules. But it after put u10 on and short SH501. it still gives a i2c write error. ( After double check the pins, looks like the pwdn pin is not set correctly, so i modified the board-mx6q_sabresd.c to force the pwdn pin to be 1. After that i2c function correct.  But still can not capture image. i did modprobe ov8820_camera_mipi & modprobe mxc_v4l2_capture. then gst-launch v4l2src num-buffers=1 ! jpegenc ! filesink location=sample.jpeg ( the camera is hooked up with /dev/video0) it shows error message

Out of memory: Kill process 6725 (gst-launch-0.10) score 577 or sacrifice child

Killed process 6725 (gst-launch-0.10) total-vm:552648kB, anon-rss:542996kB, file-rss:0kB

Killed (my system is linux kernel 3.0.35 with ltib & rootfs is ubuntu 11.10)

1 解決策
1,705件の閲覧回数
JayTu
NXP Employee
NXP Employee
1 返信
1,706件の閲覧回数
JayTu
NXP Employee
NXP Employee