about specification of the fast mode i2c signal transition.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

about specification of the fast mode i2c signal transition.

1,325件の閲覧回数
t-iishii
Contributor II

Hi,

In datasheet of i.MX6(IMX6DQCEC.pdf) section 4.11.9, 

Minimal value of Fast mode transition time specificaton(IC10, IC11) has a capacitance value as a timing parameter.

  1) Is it a input parameter? (request by i.MX6)

  2) Why does it have capacitance value as a timing parameter?

  3) If external I2C device work more faster than minimal value of this parameter,

      what kind of problems do we encounter?

  4) Both standard mode and Fast mode have different parameter for each mode.

      It seems a i2c PHY request parameter for each mode.

      If so, standard speed transfer on Fast mode, which parameter it must use?

Best regards,

Ishii.

ラベル(1)
0 件の賞賛
返信
1 返信

1,128件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please look at my comments below.

 

1.

  I2C is a bus, therefore its specifications relates for all devices,

connected to the I2C bus : masters\slaves, input \output .

 

2.

  For open drain signals (I2C, in particular) rise / fall timings depend on

capacitance load.

 

3.

  Illegal data may be taken if violation of rise / fall timings specs take place.

 

4.

  I2C masters set mode during transfer. Each transfer should satisfy its mode

specs. No standard speed transfer for Fast mode.

http://www.nxp.com/documents/user_manual/UM10204.pdf 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信