about imx8mq 4K resolution support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

about imx8mq 4K resolution support

1,906 次查看
jkshin
Contributor II

I'm developing video players with imx8mq, fsl-imx-xwayland environment.

The "imx8 gstreamer user guide" document provided by nxp states that imx8 supports waylandsink, glimagesink, and kmssink.

And the hardware reference document for the imx8mq board states that the imx8mq board supports up to 4k60p (for videos using vp9, h265 codecs).

 When the fsl-imx-xwayland kernel image is first installed, the Weston default value is 1920x1080@60, and when the 4K60p video is played with wayland sink, the frame-rate is 60fps well (in this case, of course HDMI output is 1920x1080@60).

 The problem is as follows:

 If I modify the resolution setting at /etc/xdg/weston.ini to 3840x2160@60, and play the 4K60p video with HDMI output on the 4K panel, the frame-rate drops to 30fps. Like wayland sink, the frame-rate of the glimage sink also falls, and the basic resolution of the kms sink is fixed at 1920x1080.

 

The questions are as follows.

1. Even if the imx8mq processor supports codecs for 4K60p videos, if output is supported up to 1920x1080, 4K quality videos cannot be output, right?

2. If I change the wayland default setting from 1920x1080@60 to 3840x2160@60, should I change other additional settings?

 

 

0 项奖励
回复
1 回复

1,901 次查看
joanxie
NXP TechSupport
NXP TechSupport

what display do you use? hdmi? if yes, what dtb do you use? and what resolution do you change? under the ”output“?this is for display resolution, why do you need to change this? and I remembered that imx8mq bsp comment them as default

0 项奖励
回复