about i.mx6 lvds low resolution

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

about i.mx6 lvds low resolution

1,041件の閲覧回数
浩卢
Contributor III

hi everyone

I will use lvds to output 640x480 resolution screen, but the kernel does not support 640x480 mode, how do I modify the kernel , I used the linux kernel version 3.0.101.

Thank you.

ラベル(2)
0 件の賞賛
返信
1 返信

789件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

You should try using the kernels of the official BSPs, like 3.10.53 or 3.14.38.


Additionally, you could refer to the following document from the Community, in case that you are using LVDS display:

Porting LVDS LCD With Low Resolution to i.MX6

The following thread could also be useful for you:

Frame buffer resolution in i.Mx6 Yocto

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------