about cma

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about cma

Jump to solution
706 Views
changbaoma
Contributor III

camera and display interface do not exist in my imx6ull board,but ip camera may be used.

1. can i disable the reserved-memory(cma) node in imx6ull dts? if yes, is there any bad effect?

2. which driver may use that CMA area?

0 Kudos
1 Solution
677 Views
b36401
NXP Employee
NXP Employee

I considered with collegues and it is not good idea to disable CMA.
Many peripherals on i.MX6ULL used DMA and needs CMA.
Of course you can change their drivers for not using DMA but then you loose the performance.

View solution in original post

3 Replies
694 Views
b36401
NXP Employee
NXP Employee

[deleted]

0 Kudos
685 Views
changbaoma
Contributor III

when CMA  aera enable, will all DMA transfers of imx6 Peripherals use the CMA  aera?

is there any bad effect if disable CMA node in dts?

0 Kudos
678 Views
b36401
NXP Employee
NXP Employee

I considered with collegues and it is not good idea to disable CMA.
Many peripherals on i.MX6ULL used DMA and needs CMA.
Of course you can change their drivers for not using DMA but then you loose the performance.