about bit [31: 26] of SRC_SBMR2 of i.MX 6Solo

cancel
Showing results for 
Search instead for 
Did you mean: 

about bit [31: 26] of SRC_SBMR2 of i.MX 6Solo

530 Views
Danube
Contributor IV

Hi .

We want to know more detail define in about bit [31: 26] of SRC_SBMR2 of i.MX 6Solo.

Because We setting eMMC boot in SD4 pin.

SRC_SBMR1 = 0x00005680

We know Bootable SRC_SBMR2 value is

SRC_SBMR2 (0x020D801C) = 0x22000001

We also test bootable board and remove test_mode pull down 4.7k ohm

We read SRC_SBMR2 value is


SRC_SBMR2(0x020d801c) = 0x21000001

We want to know more detail define in bit [29:28] of SRC_SBMR2.

Some fail board is show SRC_SBMR2(0x020d801c) = 0x12000001  or  0x02000001

We want to which test fail , SRC_SBMR2 is show 0x12000001  or  0x02000001 .

0 Kudos
1 Reply

415 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Apollo

bits [29:27] of SRC_SBMR2 reflects state of TEST_MODE[2:0] signals,

used for factory testing. Information about these signals are not available.

Recommended connections can be found in IMX6DQ6SDLHDG, Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applic...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos