Hello,community
I referred to datasheet of i.mx6dl about SSI timing.
In table 87, the min values of SS24,SS26,SS37~SS39 are not specified.Does it mean that these values have no lower limit(Can be a minus value)?
It seems that it is not reasonable for SS24,SS26 having a minus value.
Thank you!
ZongbiaoLiao
Actually, the minimum limit for these parameters you've listed is 0. And, you are right, they can't have a negative values.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------