about  I.MX6 linux kernel4.1 - rt18  used GPU question?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about  I.MX6 linux kernel4.1 - rt18  used GPU question?

794 Views
lvxiong
Contributor I

The SDK I used was imx-4.1-krogoth, compiled with DISTRO = fsl-imx-wayland MACHINE = imx6qsabresd source fsl-setup-release.sh-b build, compiled with bitbake fsl-image-gui.

But Linux kernel I want to add patch-4.1.15-rt18.patch on  the bsp linux4.1 kernel.  Will the GPU still work ok? Is GPU SDK specified only in version 4.1?

0 Kudos
Reply
1 Reply

708 Views
igorpadykov
NXP Employee
NXP Employee

Hi James

I believe GPU will still work ok in your case.


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply