about ADC sampling clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about ADC sampling clock

Jump to solution
1,357 Views
goto11
Contributor III

hello,Community

Can I change the ADC sampling clock during operation?
Are there any precautions when making changes?

best regards

Goto

Labels (1)
0 Kudos
Reply
1 Solution
1,226 Views
igorpadykov
NXP Employee
NXP Employee

Hi Goto

for clock usage one can look at Figure 14-2. Timing

i.MX 7Dual Applications Processor Reference Manual

Seems it is possible to change clock during operation,

valid data will be on next conversion cycle.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
1,227 Views
igorpadykov
NXP Employee
NXP Employee

Hi Goto

for clock usage one can look at Figure 14-2. Timing

i.MX 7Dual Applications Processor Reference Manual

Seems it is possible to change clock during operation,

valid data will be on next conversion cycle.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,226 Views
goto11
Contributor III

hello,

Table 93. Recommended operating conditions for 12-bit ADC in .MX 7 Dual Family of Applications Processors Datasheet
Is it OK to make the RIEXT value larger than 250Ω (for example, from several kΩ to dozens of kΩ) when FCLK and FSOC are operated at close Min values?

What kind of problems will occur if the resistance value is increased?

best regards

Goto

0 Kudos
Reply
1,226 Views
igorpadykov
NXP Employee
NXP Employee

for new questions recommended to create new thread.

Best regards
igor

0 Kudos
Reply